Part Number: PCM4220
你好,在使用TI的音频ADC PCM4220时,发现ADC转换出来的数据不稳,请TI的大咖协助分析下问题。应用电路如上图所示。在差分放大的电路的输入JS_OUT_P端给定很定的1V电压,在JS_OUT_N端给定很定的0V电压,在差分放大电路的输出(也就是PCM4220的差分输入)端可以测到的恒定差分信号(差分单端信号一个为3.16V,另一个为0.75V),但通过PCM4220采集的数据却是不断减小的数据,如下图为采集到的数字量数据曲线。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM4220
你好,在使用TI的音频ADC PCM4220时,发现ADC转换出来的数据不稳,请TI的大咖协助分析下问题。应用电路如上图所示。在差分放大的电路的输入JS_OUT_P端给定很定的1V电压,在JS_OUT_N端给定很定的0V电压,在差分放大电路的输出(也就是PCM4220的差分输入)端可以测到的恒定差分信号(差分单端信号一个为3.16V,另一个为0.75V),但通过PCM4220采集的数据却是不断减小的数据,如下图为采集到的数字量数据曲线。
您好,
不使用的右通道VINR+/VINR- 不可以接地,因为这超出了其推荐的输入范围。其单端输入峰峰值是2.8Vpp,共模电压是1.95V,也就是输入信号幅值范围是0.55V ~3.35V,不包括0V。建议VINR+和 VINR- 短接然后接VCOM(1.95V)。
另外,电路图中有两种地GNDA1和DGND,这两种地是否单点连接?
但通过PCM4220采集的数据却是不断减小的数据
建议检查I2S通信相关设置,用示波器或逻辑分析仪看下输出数据格式是否为期望形式
17和18脚是什么电平?
我理解这与您输入的模拟信号的共模电压有关,正常情况下两输入管脚的共模电压是1.95V或者说直流分量是1.95V,如下截图所示,如果直流分量不在这个1.95V电压上设备使能高通滤波器后就会一直调节这个直流分量,然后就是慢慢减小的趋势。如果您输入差分交流信号,每个管脚的共模电压是1.95V,交流信号以1.95V为中心上下摆动,那么使能高通滤波器后,不会出现慢慢减小的趋势。
以上测试您差分输入的是两个直流电压,且都不在1.95V电压上,设备会认为您输入的信号存在直流偏差,所以一直慢慢调节减小它,然后出现了以上现象。
您可以输入满足共模电压规格的差分交流信号,看采集结果是怎样的,以验证上述我的分析