Part Number: TLV320AIC3106
我想实现如下功能:通过麦克风输入把音频数据通过aic3106的i2s的dout引脚输出到主控芯片,同时把录入的音频通过主控芯片i2s输出到aic3106的LEFT_LOP和RIGHT_LOP上。
请问aic3106支持这种一边录音一边播发录音的功能吗,如果支持,路径要怎么设置,需要设置哪些寄存器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320AIC3106
我想实现如下功能:通过麦克风输入把音频数据通过aic3106的i2s的dout引脚输出到主控芯片,同时把录入的音频通过主控芯片i2s输出到aic3106的LEFT_LOP和RIGHT_LOP上。
请问aic3106支持这种一边录音一边播发录音的功能吗,如果支持,路径要怎么设置,需要设置哪些寄存器。
通过麦克风输入把音频数据通过aic3106的i2s的dout引脚输出到主控芯片,同时把录入的音频通过主控芯片i2s输出到aic3106的LEFT_LOP和RIGHT_LOP上。
您好,您说的这个过程我认为是可行的。
我同时也将您的问题提交到英文E2E上了,看是否有类似的配置示例,您可以关注他们的回复,有任何问题,可以在这里跟进我会到E2E上去跟进。