Part Number: TPA3255
我自己做了几块TPA3255的开发板,输出采用2*BTL,在调试的时候。不加输入信号,就给电路板采用+24V的电源电压供电,板子上电后直接进入欠压保护模式,即FAULT的指示灯亮,OTW指示灯不亮。经过实际测量发现,只有电压加到28.5V的时候就不报欠压保护指示了,查看芯片数据手册,供电电压低于14.5V的时候才会有欠压保护,可是我的板子低于28.5V就欠压保护,请问是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3255
我自己做了几块TPA3255的开发板,输出采用2*BTL,在调试的时候。不加输入信号,就给电路板采用+24V的电源电压供电,板子上电后直接进入欠压保护模式,即FAULT的指示灯亮,OTW指示灯不亮。经过实际测量发现,只有电压加到28.5V的时候就不报欠压保护指示了,查看芯片数据手册,供电电压低于14.5V的时候才会有欠压保护,可是我的板子低于28.5V就欠压保护,请问是什么原因?
您好,上电期间在电压还没升到14.5V之前欠压状态是正常的,直到电压抬升到阈值电压14.5V时fault才会消失。所以目前您遇到的现象是不正常的。
我想和您确认下,上电时序是否满足datasheet中Figure32的时序图,换句话说,reset在供电电压起来之前一直保持为低,TPA3255处于高阻态时,供电电压上升期间,fault也是等到24.5V时才拉高吗?