Part Number: TLV320AIC3110
Other Parts Discussed in Thread: TS3A5223
小白请教如何使用TLV320AIC3110输出两路headphone;
原自带一路headphone driver,即如何将class D speaker driver 输出转换为headphone输出,接3.5mm耳机,电路怎么设计?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320AIC3110
Other Parts Discussed in Thread: TS3A5223
小白请教如何使用TLV320AIC3110输出两路headphone;
原自带一路headphone driver,即如何将class D speaker driver 输出转换为headphone输出,接3.5mm耳机,电路怎么设计?
您好,AIC3110专门设计为一路headphone driver,和一路speaker output 的应用。
所以如果您需要headphone 输出,我想最好还是选择多路headphone输出的codec直接使用。
我看了下比如AIC3204,AIC3254,一路line output,一路headphone output,内部架构都是一样的,所以line output这里应该也是可以接headphone output的。

感谢您的回复,
如果headphone输出只需要支持二选一,请问选用TS3A5223这颗模拟开关,分别将左右声道1:2输出,是否合适?
您好,TS3A5223是2选1开关,不能做扇出,即1路输入2路输出的应用。
数据手册中对于开关描述2:1或者1:2 是因为IO口是双向的,既可以作为输入也可以作为输出,但功能只能是2选1.
您好,明白。我的应用只需要输出是2选1的,即TLV320AIC3110 headphone out -> TS3A5223 -> 2路耳机输出,耳机输出可以2选1切换
但是TLV320AIC3110 headphone out 是一路headphone输出,一路speaker输出。
TLV320AIC3110 的一路headphone out无法通过TS3A5223实现2路输出。
所以TLV320AIC3110 headphone out -> TS3A5223 -> 2路耳机输出。这里我理解的您是想通过TS3A5223实现1路耳机输入,2路耳机输出的目的是吗?
TLV320AIC3110 的1路耳机输出,通过TS3A5223 接到2个耳机上,这两个耳机不需要同时有声音,可以随时切换就可以
那是可以的,AIC3110的1路耳机和TS3A5223 的其中一路选通。