Hello,
I am trying to program the DRC on the TAS5713.
The documentation says the threshold is in 9.23 format and the other coefficients are in 3.23 format.
I notice that the threshold parameter fetch in the chip manual was not explicitly mentioned ,when using gui simulation ,I
converted db to 9.23 format,but the resulting value is not the same as the gui displayed value.At the same time,3.23 conversion
of softening filter and the values of attack and release is not correct.I want to know the calculation formulas of these parameters