This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

音视频分配器电路设计

想做一个音视频分配器,但是在网上都搜不到相关资料,想问各位老师有没有相关资料,电路等等...

l.任务要求

设计一种1路输入4路输出的音视频分配器电路。

   2.性能指标要求:

(1).音频频响50Hz-20KHz; 音频输入: 最小电平0.4 VP-P最大 6.0 VP-P;  音频输出:最小电平0.4 VP-P最大 6.0 VP-P;   输入输出阻抗:600Ω±6Ω

(2)视频频响:10Hz-6MHz ;视频输入: 最小电平0.4VP-P,最大 2 VP-P;  视频输出:最小电平0.4 VP-P,最大 2 VP-P;   输入输出阻抗:75Ω±1Ω

    实际电路的供电电压为交流220V,原理电路、印制板电路要体现。