This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

音频编解码器相关问题

您好!

最近因为项目需要,现在需要选择一款芯片,主要思路是:通过TI DSP2812与DAC芯片连接产生4KHZ左右的正弦波,然后将4KHZ的正弦波经过AD转换再传回到DSP2812中,检查数据的变化(主要是检测相位变化)。我想选择一款芯片,看见有款TLV320AIC23的芯片,可以实现AD、DA集成于一个芯片上,可是感觉太复杂了,我想询问一下TI有没有其他型号的芯片可以实现我上面说的功能?谢谢!
             还有一点小疑问:DSP发送数据时通过外扩DA芯片产生4KHZ正弦波,接收时用DSP自带的AD接收数据,是不是没法实现?(我这样设计了,试了下,感觉不对,可是还是不太明白原因。)

  • 能提供一下具体参数要求吗?比如对精度的要求,正弦波的峰峰值有什么要求。

    当然,不清楚你对信号质量的要求,但是普遍意义来说,“通过外扩DA芯片产生4KHZ正弦波,接收时用DSP自带的AD接收数据”是可以实现的,中间的信号调理需要根据你选用的DAC以及DSP自带的ADC的参数来决定。