This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3110D2无信号输入,输出的载波信号有毛刺

  1. 采用评估板电路,两级LC滤波,12V电源供电,无信号输入时,输出的正弦波信号有轻微的毛刺,是PCB布板的问题吗?接8欧姆无感负载,输入12kHz信号,听到高频鸣叫,是电感发出的声音?

  2. 采用12V电源,功率输出大约是5W,调节gain0,gain1的电平,可以增大功率吗?

 谢谢!

  • 我觉得:

    无输入信号时,输出不会有正弦波吧。

    12kHz那个应该是电感的声音。

    12V5W,增大增益,可以增大功率。前提是你的PLIMIT功能没有限功率。

  • 有个336KHz的正弦波信号

    增大增益,功率增大但是失真了,也就是说最大功率还是没有变

  • 你好:

    1.你应该是看的单通道的输出,differential的输出,也就是负载两端就没有这个正弦波信号。

    因为线路上有寄生参数,所有无信号输入的时候,输出的50%占空比的方波上会有过冲和振铃。过了LC电路就会出现和开关频率一样的正弦波信号。

    2.增大增益如果信号失真的话,你先检查一下电源的功率够不够。然后你是单端接法还是BTL接法,看下是否受电源电压的限制,提高供电电压会不会改善。

    还有Plimit的电压是不是接上了。