This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想问一下,TLV320AIC23B这款芯片内部模拟通道有加滤波器吗?有的话,滤波器大致的响应是怎么样的,截止频率点是多少?在使用时,是否需要在模拟信号的输出和输入通道再加滤波器?
不知道你说的是不是指这个?
All performance measurements done with 20-kHz low-pass filter and, where noted, A-weighted filter.
我看到datasheet上写的LINEIN部分里有Active and passive filters for the two channels prevent high frequencies from folding back into the audio band这句话,在LINEOUT部分里有The DAC is connected to the line outputs via a low-pass filter that removes out-of-band components. No further external filtering is required in most applications.因此想确认一下是不是芯片内部模拟通道都有滤波器了,有的话滤波器响应是怎么样的?还需要自己再加滤波器吗?
其实主要是想知道,音频芯片TLV320AIC23B在音频模拟信号输入时在LINEIN前需不需要加抗混叠滤波器,如果要加的话,因为A/D用的是sigma-delta过采样技术,所以是不是可以把截止频率设计的高一点