Part Number: LM833
Other Parts Discussed in Thread: ADS8688
如图,高增益带宽积产品
详细参数
问题1:请问下GBW本身代表增益带宽积,为16MHz
下面的单位增益频率 B1 9MHz是个什么意思?
问题2:这个是开环的幅频特性图吗?为什么只有60dB?
问题3:LM833不是单位增益稳定吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
1、单位增益频率9MHZ 是开环增益频率特性曲线中(所截图表格中测试条件写了open loop),当开环增益下降到0db时对应的频率,从figure 26可以看出是9MHZ。
2、是的,是开环的幅频特性图;
为什么只有60dB?
我们知道运放包含一个极点时,运放的增益带宽积与单位增益带宽相等,而对于LM833 ,这两个参数是不相等的,因此LM833应该包含2个或2个以上的极点。
我们看datasheet 给出的开环幅频曲线,它是从1KHZ开始的,因此在0~1KHZ之间应该还存在一个极点即运放的第一个极点,而在这个第一个极点之前,其开环增益应该是比较高的,最起码大于60dB。
我在datasheet中想找的其直流开环增益Aol,但是没有找到,我找到了参数AVD,LM833 是比较老的产品了,它没有使用我们经常看的Aol。Aol与区别可以在下面链接找到:
因此其低频开环增益在25℃可以到110dB。

3、LM833 单位增益稳定。
谢谢解答。
想用这个做12.4kbps数据刷新率的SAR型ADC前面的缓冲,ADC采用ADS8688,这个缓冲时时单位增益跟随的方式,所以关心了下上面几个参数,只要单位稳定,估摸着能用。