This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用USB音频桥为TAS5825M提供I2S信号,再通过MCU配置完TAS5825M后读取其寄存器数值,发现reg57(0x39)即 CLKDET_STATUS Register显示为0b1000报错,datasheet中指示错误为(:This bit indicates whether the PLL is locked or not. The PLL is reported as unlocked when the PLL is disabled.)。
此时,I2S信号在48khz/24bit 44.1khz/24bit是可正常播放声音的,但是当通过PC端将I2S信号手动切换为48khz以上采样率(如96khz/192khz)后,TAS5825M便输出直流信号,不能正常播放声音。经查,I2S信号正常,其在PCM1794上使用高于48khz的采样率时可正常播放声音,所以只可能是TAS5825M的问题。请问这应该如何解决?
您好,您是使用的PPC3 EVMGUI配置的采样率吗?如果是IO口使用USB的话,是只能支持到48Khz的,要到Audio In那里从PPCMB切换到PSIA。
请参考这个帖子,和您的问题类似:
我没有取得PPC3 EVMGUI的许可,于是根据数据手册上的寄存器配置,在寄存器页面我没有找到设置AudioIn的寄存器页面。申请PPC3的页面提示我需要使用工作邮箱发送,但是我现在是本科生并没有工作邮箱,我有什么办法可以取得这个许可证吗?