Part Number: PCM1792A
如题,PCM1792A在没有I2S信号LRCK、BCK、DATA和SCK输入时,即没有SCK时钟信号,能否用I2C模式读写内部设置寄存器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
再有系统复位要经过1024个SCK周期,是否没有SCK就不能复位,
是的;但是我认为这里不进行复位,I2C接口应该也能用。I2C通信时,RST管脚是否拉高了?供电电压也检查下是否都正常?
SCK也算I2S的一部分吧
不算,音频接口包括LRCK (pin 4), BCK (pin 6), and DATA (pin 5),但要求LRCK 与SCK同步:

I2C接口是OD接口需要接上拉,您是否接上拉?

检查下I2C主控端输入和输出电平是否与PCM兼容?

看 datasheet I2C接口处描述,没有说需要SCK时钟信号,您检查上述几点没问题后,如果I2C还是没有ACK,您输入SCK再看下I2C是否有ACK?