This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3251: BTL模式下输出异常

Part Number: TPA3251


您好:我在使用TPA3251时遇到了两个输出异常的问题:

1)TPA3251在采用BTL模式时,出现27,28脚无PWM信号输出,其他输出脚的PWM输出信号均正常,且一路通道可以正常播放声音,确认该网络的偏置电压明显小于其他输出网络,且对地阻抗也与其他输出网络不同。拆解下IC后单独确认这四个输出网络的引脚与IC的GND之间阻抗时,四个网络时一致的。把该IC更换至其他新的PCB板后现象复现。

2)同样采用BTL模式的TPA3251,四个输出网络的PWM信号出现时有时无现象。在不重新上电的情况下,四个网络均是一会可以正常输出信号,一会就完全无信号输出了。且该IC更换至其他PCB板上后现象完全一致。

以上两个出现问题的IC分别可能出现什么原因呢?