Part Number: PCM1864
Dear developer:
HI~
I have a question about PCM1864 slave address in devices tree. The real slave address should be "0x94" or "0x4a" that I setting in devices tree?
sincerely
Jeper 2023.11.10
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,应该位0x94.
当adress pin为low时,7bit从机地址为1001 010
I2C的时序格式为: Start+7bit address+R/W bit。 因此第八位为读写位,所以8bit地址位1001 0100,即0x94.