Other Parts Discussed in Thread: TPA3113D2
请教工程师们一个问题:
我手头有一款音频Codec且集成了2W D类功放,但是需求要求音频输出功率5W,我在此Codec输出基础上增加一级功放,增加的功放的功率为3W,请问最终输出的功率是多少?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
这样我想最终还是3W。
对于一个最大功率是3W的功放来说,如果负载是4ohms,输出电压最大为3.4Vrms,受供电电压及内部结构的限制,输出电压会限制在3.4Vrms。(如果负载时8ohms,电压就不同)。即使前级的输入信号增大,输出也会限制在3W。
建议直接接在codec的line out输出口,接5W的功放。
5W的功放可以使用TPA3113D2。