Part Number: OPA1612
Other Parts Discussed in Thread: TL072,
,芯片温度很高,两片1612电流在350mA左右, 我的供电是正负15V ,电源部分都是正常的, 我换成TL072电路可以正常。
但我觉得OPA1612性能会好一些,所以选择这个芯片,为何会不适合这个电路呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,看了下您的电路,有两点疑问:
1)C9在这里的作用是什么?看下两个运放的输出端是否短路了,造成两个输出端由于电压不同形成的回路大电流,从而导致功耗增大。
2)滤波器的架构是MFB filter吗?如果是MFB架构,两个反馈电容接在R41和R42前面是对的,但是反馈电阻R43和R44应该接在R41和R42的外面。
MFB filter的架构如下: