This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2912a做的USB声卡出现unknown device

测了一下,晶振没起振,

VBUS为5V , 

VCCP , VCCA , VCCR , VCCL , VDD均为3.3V,

BGND , PGND , HGND , DGND , GND , AGND均为0V ,

MBIAS为0.7V,

晶振两端用示波器侧没有信号也没有直流电压,用万用表测是2.3V,

测试时只焊了USB到芯片的D+,D-上的33Ω电阻和D+的1.5k上拉,晶振和晶振两端的电容以及晶振两脚之间的1M的电阻,还有所有的电源到地的滤波电容,其他的元件暂时没有焊。

目前还没有找到问题所在。