This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5509的 AIC23 语音芯片问题

我测试了一下5509的codec程序,playmode选择为1,通过line in 输入,phone out输出声音,语音芯片为aic23,在debug的时候,点击暂停,依然会播放声音?还有如何将mcbsp的内容写到dma的rcv里面和将dma的xmt内容写到mcbsp上?如何让AIC23播放DMA的xmt里面的内容?

下面是程序代码

 

/******************************************************************************/


/*----------------------------------------------------------------------------*/
/* DESCRIPTION:                   */
/*                       */
/* This is an example for EMIF of C5509            */
/*----------------------------------------------------------------------------*/
/* MODULE NAME... I2C and Mcbsp              */
/* FILENAME...... codec.c                 */
/* DATE CREATED.. Mon 02/4/2004                 */
/* COMPONENT.....                  */
/* PREREQUISITS..                  */
/*----------------------------------------------------------------------------*/
/* DESCRIPTION:                  */  
/*                       */
/* this example is that the codec is controled by the I2C and Mcbsp     */
/*----------------------------------------------------------------------------*/

#include <csl.h>
#include <csl_i2c.h>
#include <stdio.h>
#include <csl_pll.h>
#include <csl_mcbsp.h>

#define CODEC_ADDR 0x1A

 

/*锁相环的设置*/
PLL_Config  myConfig      = {
  0,    //IAI: the PLL locks using the same process that was underway 
                //before the idle mode was entered
  1,    //IOB: If the PLL indicates a break in the phase lock, 
                //it switches to its bypass mode and restarts the PLL phase-locking 
                //sequence
  12,    //PLL multiply value; multiply 24 times
  1             //Divide by 2 PLL divide value; it can be either PLL divide value 
                //(when PLL is enabled), or Bypass-mode divide value
                //(PLL in bypass mode, if PLL multiply value is set to 1)
};

unsigned int play_mode;   // 0:play     1:record and play

MCBSP_Config Mcbsptest;

/*McBSP set,we use mcbsp1 to send and recieve the data between DSP and AIC23*/
MCBSP_Config Mcbsp1Config = {
  MCBSP_SPCR1_RMK(
    MCBSP_SPCR1_DLB_OFF,                   /* DLB    = 0,禁止自闭环方式 */
    MCBSP_SPCR1_RJUST_LZF,                 /* RJUST  = 2 */
    MCBSP_SPCR1_CLKSTP_DISABLE,            /* CLKSTP = 0 */
    MCBSP_SPCR1_DXENA_ON,                  /* DXENA  = 1 */
    0,                                     /* ABIS   = 0 */
    MCBSP_SPCR1_RINTM_RRDY,                /* RINTM  = 0 */
    0,                                     /* RSYNCER = 0 */
    MCBSP_SPCR1_RRST_DISABLE               /* RRST   = 0 */
   ),
    MCBSP_SPCR2_RMK(
    MCBSP_SPCR2_FREE_NO,                   /* FREE   = 0 */
    MCBSP_SPCR2_SOFT_NO,                   /* SOFT   = 0 */
    MCBSP_SPCR2_FRST_FSG,                  /* FRST   = 0 */
    MCBSP_SPCR2_GRST_CLKG,                 /* GRST   = 0 */
    MCBSP_SPCR2_XINTM_XRDY,                /* XINTM  = 0 */
    0,                                     /* XSYNCER = N/A */           
    MCBSP_SPCR2_XRST_DISABLE               /* XRST   = 0 */
   ),
   /*单数据相,接受数据长度为16位,每相2个数据*/
  MCBSP_RCR1_RMK( 
   MCBSP_RCR1_RFRLEN1_OF(1),              /* RFRLEN1 = 1 */
   MCBSP_RCR1_RWDLEN1_16BIT               /* RWDLEN1 = 2 */
  ),
  MCBSP_RCR2_RMK(    
    MCBSP_RCR2_RPHASE_SINGLE,              /* RPHASE  = 0 */
    MCBSP_RCR2_RFRLEN2_OF(0),              /* RFRLEN2 = 0 */
    MCBSP_RCR2_RWDLEN2_8BIT,               /* RWDLEN2 = 0 */
    MCBSP_RCR2_RCOMPAND_MSB,               /* RCOMPAND = 0 */
    MCBSP_RCR2_RFIG_YES,                   /* RFIG    = 0 */
    MCBSP_RCR2_RDATDLY_1BIT                /* RDATDLY = 1 */
    ),  
   MCBSP_XCR1_RMK(    
    MCBSP_XCR1_XFRLEN1_OF(1),              /* XFRLEN1 = 1 */ 
    MCBSP_XCR1_XWDLEN1_16BIT               /* XWDLEN1 = 2 */
    
 ),   
 MCBSP_XCR2_RMK(   
    MCBSP_XCR2_XPHASE_SINGLE,              /* XPHASE  = 0 */
    MCBSP_XCR2_XFRLEN2_OF(0),              /* XFRLEN2 = 0 */
    MCBSP_XCR2_XWDLEN2_8BIT,               /* XWDLEN2 = 0 */
    MCBSP_XCR2_XCOMPAND_MSB,               /* XCOMPAND = 0 */
    MCBSP_XCR2_XFIG_YES,                   /* XFIG    = 0 */
    MCBSP_XCR2_XDATDLY_1BIT                /* XDATDLY = 1 */
  ),            
 MCBSP_SRGR1_DEFAULT,
 MCBSP_SRGR2_DEFAULT,  
 MCBSP_MCR1_DEFAULT,
 MCBSP_MCR2_DEFAULT, 
 MCBSP_PCR_RMK(
   MCBSP_PCR_IDLEEN_RESET,                 /* IDLEEN   = 0   */
   MCBSP_PCR_XIOEN_SP,                     /* XIOEN    = 0   */
   MCBSP_PCR_RIOEN_SP,                     /* RIOEN    = 0   */
   MCBSP_PCR_FSXM_EXTERNAL,                /* FSXM     = 0   */
   MCBSP_PCR_FSRM_EXTERNAL,                /* FSRM     = 0   */
   0,                                      /* DXSTAT = N/A   */
   MCBSP_PCR_CLKXM_INPUT,                  /* CLKXM    = 0   */
   MCBSP_PCR_CLKRM_INPUT,                  /* CLKRM    = 0   */
   MCBSP_PCR_SCLKME_NO,                    /* SCLKME   = 0   */
   MCBSP_PCR_FSXP_ACTIVEHIGH,              /* FSXP     = 0   */
   MCBSP_PCR_FSRP_ACTIVEHIGH,              /* FSRP     = 1   */
   MCBSP_PCR_CLKXP_FALLING,                /* CLKXP    = 1   */
   MCBSP_PCR_CLKRP_RISING                  /* CLKRP    = 1   */
 ),
 MCBSP_RCERA_DEFAULT, 
 MCBSP_RCERB_DEFAULT, 
 MCBSP_RCERC_DEFAULT, 
 MCBSP_RCERD_DEFAULT, 
 MCBSP_RCERE_DEFAULT, 
 MCBSP_RCERF_DEFAULT, 
 MCBSP_RCERG_DEFAULT, 
 MCBSP_RCERH_DEFAULT, 
 MCBSP_XCERA_DEFAULT,
 MCBSP_XCERB_DEFAULT,
 MCBSP_XCERC_DEFAULT,
 MCBSP_XCERD_DEFAULT,  
 MCBSP_XCERE_DEFAULT,
 MCBSP_XCERF_DEFAULT,  
 MCBSP_XCERG_DEFAULT,
 MCBSP_XCERH_DEFAULT
};     
/* This next struct shows how to use the I2C API */
/* Create and initialize an I2C initialization structure */
I2C_Setup I2Cinit = {
        0,              /* 7 bit address mode */
        0,         /* own address - don't care if master */
        84,            /* clkout value (Mhz)  */
        50,            /* a number between 10 and 400*/
        0,              /* number of bits/byte to be received or transmitted (8)*/
        0,              /* DLB mode on*/
        1               /* FREE mode of operation on*/
};

I2C_Config testI2C;


/*数字音频接口格式设置
AIC23为主模式,数据为DSP模式,数据长度16位*/   
Uint16 digital_audio_inteface_format[2]={0x0e,0x53};
/*AIC23的波特率设置,采样率为44.1K*/
Uint16 sample_rate_control[2] = {0x10,0x23};
/*AIC23寄存器复位*/
Uint16 reset[2] ={0x1e,0x00};
/*AIC23节电方式设置,所有部分均所与工作状态*/
Uint16 power_down_control[2] ={0x0c,0x03};
/*AIC23模拟音频的控制
DAC使能,ADC输入选择为Line*/
Uint16 analog_aduio_path_control[2] ={0x08,0x10};
/*AIC23数字音频通路的控制*/
Uint16 digital_audio_path_control[2] ={0x0a,0x05};
/*AIC23数字接口的使能*/
Uint16 digital_interface_activation[2] ={0x12,0x01};
/*AIC23左通路音频调节*/
Uint16 left_line_input_volume_control[2] ={0x00,0x17};
/*AIC23右通路音频调节*/
Uint16 right_line_input_volume_control[2] ={0x02,0x17};
/*AIC23耳机左通路音频调节*/
Uint16 left_headphone_volume_control[2] ={0x05,0xFF};
/*AIC23耳机右通路音频调节*/
Uint16 right_headphone_volume_control[2] = {0x07,0xFF};
/*定义McBSP的句柄*/
MCBSP_Handle hMcbsp;

Uint16 i2c_status;
Uint16 i,temp;

 

void delay(Uint32 k)
{
   while(k--);
}


void main(void)
{

    Uint16 aic23data = 0;


 i2c_status = 1;
 play_mode=1; 
    /* Initialize CSL library - This is REQUIRED !!! */
    /*初始化CSL库*/
    CSL_init();
 
 /*设置系统的运行速度为140MHz*/
    PLL_config(&myConfig);
    
    /* Initialize I2C, using parameters in init structure */
    /*初始化I2C的格式*/

// I2C_config(&Config);
// I2C_start();
 
// I2C_getConfig(&Config1);
 /*I2C is undet reset*/
 I2C_RSET(I2CMDR,0);
 /*设置预分频寄存器,I2C的mode clock is 10MHz*/
 delay(100);
 I2C_RSET(I2CSAR,0x001A);
 I2C_RSET(I2CMDR,0x0620);
  
    I2C_setup(&I2Cinit);
   /*设置I2C的Mater clock*/
 I2C_RSET(I2CCLKL,100);
 I2C_RSET(I2CCLKH,100);

    I2C_getConfig(&testI2C);

 /*初始化McBSP0*/
 hMcbsp = MCBSP_open(MCBSP_PORT1,MCBSP_OPEN_RESET);
 /*设置McBSP0*/
 MCBSP_config(hMcbsp,&Mcbsp1Config);
 /*启动McBSP0*/
 MCBSP_start(hMcbsp, 
                MCBSP_RCV_START | MCBSP_XMIT_START, 
                0);

    MCBSP_getConfig(hMcbsp,&Mcbsptest);

    /*reset AIC23*/
    i2c_status = I2C_write( reset,          //pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                   ); 
 delay(1000);
    /*设置AIC23各部分均工作*/
    i2c_status = I2C_write( power_down_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                   );            
 /*设置AIC23的数字接口*/
 i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                      );
  /*设置AIC23模拟通路*/
/* i2c_status = I2C_write( analog_aduio_path_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                   );*/
 /*设置数字通路*/
 i2c_status = I2C_write( digital_audio_path_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                     );     
 /*设置AIC23的采样率*/
 i2c_status = I2C_write( sample_rate_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                      );
 /*设置耳机音量*/
 i2c_status = I2C_write( left_headphone_volume_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                      );
 i2c_status = I2C_write( right_headphone_volume_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                      );  
 /*设置Line输入的音量*/
 i2c_status = I2C_write( left_line_input_volume_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                      );
 i2c_status = I2C_write( right_line_input_volume_control,//pointer to data array
                      2,    //length of data to be transmitted
                      1,    //master or slaver
                      CODEC_ADDR,     //slave address to transmit to
                      1,    //transfer mode of operation
                      30000   //time out for bus busy
                      );
 /*启动AIC23*/
 i2c_status = I2C_write( digital_interface_activation,//pointer to data array
         2,    //length of data to be transmitted
         1,    //master or slaver
         CODEC_ADDR,     //slave address to transmit to
         1,    //transfer mode of operation
         30000   //time out for bus busy
         );
         
 /*回放音频*/
 while(TRUE)
 {


 
 if(play_mode==1)  //record and play
 {
  while(!MCBSP_xrdy(hMcbsp)){};
  aic23data = MCBSP_read16(hMcbsp);
  for(temp=3000;temp>0;temp--);
  while(!MCBSP_rrdy(hMcbsp)){};
  MCBSP_write16(hMcbsp,aic23data);
 }
 else
 {
  
  while(!MCBSP_rrdy(hMcbsp)){};
         
  aic23data = 5000;

  for(temp=30000;temp>0;temp-=100)
        {
         for(i=0;i<2;i++)
        {
           aic23data = 5000;
           MCBSP_write16(hMcbsp,aic23data);       
           delay(temp);
           aic23data = 0;
           MCBSP_write16(hMcbsp,aic23data);        
           delay(temp);
   }
        }
  
 }
  //MCBSP_write16(hMcbsp,aic23data);  
 }; 
                                  
}


void Delay(unsigned int nDelay)
{
 unsigned int ii,jj,kk=0;
 for ( ii=0;ii<nDelay;ii++ )
 {
  for ( jj=0;jj<2048;jj++ )
  {
   kk++;
  }
 }
}


/******************************************************************************\
* End of i2c2.c
\**********************

  • 暂停后依然会播放声音?  要不命令没有执行, 要么是数据缓冲的问题.因为播放芯片的缓冲里还留有一定的数据可以继续播放一会

  • 是的,暂停依然会继续播放 Line in输入的数据

    命令为什么会没执行?还有就是在debug模式下,我单步调试,发现在

     /*设置AIC23的数字接口*/
     i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array
                          2,    //length of data to be transmitted
                          1,    //master or slaver
                          CODEC_ADDR,     //slave address to transmit to
                          1,    //transfer mode of operation
                          30000   //time out for bus busy
                          );

    这一步就开始播放声音了,还没有到main函数,这又是为什么?