This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5431-Q1: IN_P/IN_N输入问题

Part Number: TAS5431-Q1

现使用R2R电阻网络实现DAC功能,接功放TAS5431驱动4W扬声器,原理图如上,请问:

1、IN_P/IN_N内部偏置电压为3V,是否需要控制IN_P输入电压小于3V,否则是否会出现满偏,导致音频失真?

2、R2R网络输出阻抗1k,下一级输入阻抗至少大于1MΩ才能保证输出稳定,不被拉偏,TAS5431为D类功放,内部集成比较器,R2R输出是否可以串电容连TAS5431?是否需要外部增加运放跟随?

  • 您好,我现在看下您的问题,尽快给您答复。

  • IN_P/IN_N内部偏置电压为3V,是否需要控制IN_P输入电压小于3V,否则是否会出现满偏,导致音频失真?

    这里的3V指的是直流偏置,也就是说IN_P和IN_N是以3V为参考的信号。比如IN_P幅值为2V的话,以3V为参考,即1V~4V的信号。

    R2R网络输出阻抗1k,下一级输入阻抗至少大于1MΩ才能保证输出稳定,不被拉偏,TAS5431为D类功放,内部集成比较器,R2R输出是否可以串电容连TAS5431?是否需要外部增加运放跟随?

    下面是输入阻抗和增益的关系,可以看到当Gain为20dB时输入阻抗最大为60Kohm。 如果要求下一级阻抗大于1M才能稳定的话, 建议使用运放做跟随。

    另外,TAS5431输入一定要AC耦合输入,这样避免前端输出有直流偏置,通过AC耦合电容将这个直流偏置隔离掉,而TAS5431输入INP和INN内部已经 集成了3V偏置,所以也就不需要再额外添加偏置电路,直接连接就好。