在用TAS5715时候会在7K附件THD变大,其它频点正常?我修改了输出LC的电感值,降下来了,不知道为什么会对THD有影响,能否解释下?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在用TAS5715时候会在7K附件THD变大,其它频点正常?我修改了输出LC的电感值,降下来了,不知道为什么会对THD有影响,能否解释下?
2%太大了,电感饱和了?电容用的瓷片是什么等级的,不要用Y等级的。
我的RC有加上,按照参考设计3.3R阻和10nF电容,需要怎么更改下
还有,你说的高频环流,是不是功放的PWM振荡频率384k会传导出来?
还有个问题我们的低频50hz左右最大功率的时候,失真在3%,正常吗?能否解释下为什么低频失真会比较大?
提供以下几方面数据:
1. 50Hz,THD vs output扫描曲线,使用电阻作为负载,不要用扬声器;
2. 10W,THD vs 频率扫描曲线,电阻负载;
3. 你的原理图;
4. 使用的电感资料。
你好:
低频段THD+N比较大,是因为这个时候noise占主导。你在50HZ的时候THD+N比较大,有可能是引入了工频噪声,你检查一下电源是否有隔离。