This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVAIC3101 I2S配置问题

w 30 13 04     # 连接MIC1LP到 L-PGA,MIC1设置为单端输入模式,L-ADC上电

w 30 18 00     # 同时连接MIC1LP到R-PGA

w 30 16 04     # R-ADC上电

w 30 19 40     # 麦克风偏置电压为2.5V

w 30 0F 34     # L-PGA增益设定为26dB

w 30 10 34     # R-PGA增益设定为26dB

硬件上是MIC1LP和MIC1LM输入

我现在按上面的设置,测试I2S输出信号波形,I2S左声道没有输出。 

只设置MIC1LP连接到L-ADC,还是只有I2S右声道有信号

 

请问是有什么原因吗