Part Number: TAS5805M
请问TAS5805M如何设置到10W以内?我们的喇叭功率最大只支持10W,TAS5805M是可以到20W吧?现在大音量时有很强的暴破音,小音量时就没有。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS5805M
请问TAS5805M如何设置到10W以内?我们的喇叭功率最大只支持10W,TAS5805M是可以到20W吧?现在大音量时有很强的暴破音,小音量时就没有。
输出配置为BTL 模式还是PBTL 模式?
BTL配置下,输出功率达到20W的测试条件如下:

如果是PBTL配置下,输出达到20W以上的测试条件如下:

Hi,Kailyn Chen
上面提到的2个问题,帮忙指导下,谢谢!
1、TAS5805M 输出幅值过大,一直在29.5V左右,看规格书说设置54寄存器可调整,但实际设置了没有起作用,其他寄存器,如音量控制寄存器4C,设置后也只能改变音量大小,输出的电压幅值没有变化,如果想让输出幅值变小,要如何设置寄存器呢?
2、输出的波形比较奇怪,不是正弦波,我们用了多种频率的音频,1KHZ、2KHZ。。。等等,波形都一样奇怪,图片已贴在上一楼,帮忙看下如何优化这个波形。
靠近芯片输出引脚这里波形是平滑的,不像上面信号失真严重,方波可能是因为analog gain设置的太大,导致输出削波。
另外,您可以读取下fault registers 0x70~0x75,看是否有报错现象。
0x70-75读出来都是0

另外,54寄存器我看写成功了,读出来也是我写入的0x0A,但实际输出电压并无变化,还是29V左右,看规格书,就是设置54可以调整output输出电压值,实际设置却是无效的,这是什么原因呢