Part Number: OPA2134
我设计了一个类似单刀双掷机械开关的电路,可以实现单片机引脚控制±9V同时开通或关断,如下图所示。

现在我想用这个电路控制的±9V给OPA2134供电,但仿真后它们并不是同时开通和关断的,开通时差在微秒级,关断时差在毫秒级,见下图,不知道会不会损坏OPA2134?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,OPA2134能正常工作的供电电压范围为+-2.5V~+-18V,即单电源5V~36V。
如果正负电压不同时开通和关断,压差在这个范围内就能保证不会损坏。
如果超过了36V,那么芯片会由于过应力的影响导致芯片损坏。