This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4950: 器件在BTL模式下驱动8Ω喇叭,应该怎么选择喇叭的功率

Part Number: LM4950

各位专家,我现在遇到如下问题:

在使用LM4950的过程中我选择连接8Ω额定功率为2W的喇叭作为输出,连接方案为数据手册中推荐的BTL模式,但在使用中功放芯片烧毁,喇叭阻抗变为0Ω。

针对上面现象,想咨询几点问题:

1.LM4950烧毁是否是外接负载过低导致?

2.LM4950BTL输出功率为7.5W,那对于喇叭应该如何匹配功率?

 

麻烦解答一下,谢谢!

  • 您好,

    明天或后天我会具体看下你的问题,若给你带来不便很抱歉。

  • 您好,

    首先很抱歉现在才回复你的问题。

    有可能是外接负载阻抗过低导致,LM4950BTL输出功率应与喇叭额定功率匹配,但应小于喇叭的最大功率。

  • 1.LM4950烧毁是否是外接负载过低导致?

     8欧2W的喇叭,负载阻抗没问题,而有可能是你的喇叭功率太小,你让功放输出功率过大,音圈烧毁短路造成功放芯片损坏。可我查询规格书,该芯片有短路保护,即使负载为0也应该是功放芯片进入保护才对,也不至于烧毁功放芯片。所以还得更换合适功率的喇叭看看是否是因为喇叭烧毁短路造成的功放烧毁。

    2.LM4950BTL输出功率为7.5W,那对于喇叭应该如何匹配功率?

    这个看如何应用,HiFi圈有句说法,用最低四倍的功率去推喇叭,也就是你7.5W的功放去推2W的喇叭是没有任何问题的,原则是你不要满功率失真去推。通常消费类的做法,是功放输出多少功率,就选择功放输出功率等同功率的或者大于功放输出功率的喇叭。当然喇叭阻抗要和功放输出的额定阻抗匹配。

  • 感谢你的分享~