This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在TAS5828M的寄存器列表中,64h中GPIO_RESETZ_SEL的具体作用是什么?是01h寄存器中的两种RST控制其中的一种,还是有单独的作用。
另外64h该功能说明中“GPIO0 can not be reset by GPIO reset”是什么意思,用GPIO1和GPIO2做该功能的时候,与GPIO0不一样吗?
您好
1、GPIO_RESETZ_SEL这个是选择哪个管脚有reset功能
根据datasheet中如果您配置管脚功能了,这个reset属于如图标识的这种。
2、GPIO0有一个端口复用功能是FAULT,因为这个功能下是DO的属性,很多客户需要这个管脚来辅助客户判断问题,所以不建议您将这个管脚配置相关Reset功能。
如果将GPIO0配置为FaultZ,GPIO1配置为Reset。
GPIO0报FaultZ状态,此时用GPIO1进行Reset,是不会复位GPIO0的FaultZ状态的是吗
您好
依据datasheet说明,以GPIO0为例,它既可以做故障报错用的管脚也可以做复位管脚,但是不可以同时。所以在使用中不建议将故障报错管脚配成复位管脚。这个配置说明的是在复位过程中不复位报错管脚这样可以留下相关报错日志,您可以通过这个记录来进一步改善或者优化这个系统。