This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1808: 模拟输入短接到GND,I2S数据管脚还一直输出数据,底噪数据

Part Number: PCM1808

各位大佬,请教个问题。使用了官方给的PCM1808的光绘文件做了demo板,把模拟输入L/R通过电容短接到GND。此时测量SDOUT管脚有波形,所以采集到SOC就会有些噪音。给的输入DC是5.09V,电源纹波是23mv;LDO输出的3.3V的纹波是20mv;测量VREF电压是2.534V,L声道上电压是2.518,R声道上电压是2.515V. 

x 出现错误。请重试或与管理员联系。