This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5102A: PCM5102A XSMT直接上拉到DVDD是否可以

Part Number: PCM5102A


你好,下图是我使用PCM5102A设计的数字音频转换器的原理图,想问下是否存在问题,主要是XSMT是否可以上拉到1.8V的DVDD,I2S输入时1.8V的数字信号

  • 您好,

    XSMT是控制是否mute的控制信号,正常时连接外部CPU或者其他控制器的。这个信号是3.3V电平的,1.8V是不可以的。

    如果你不用这个信号,datasheet里也建议:In systems where XSMT is not required, it can be directly connected to AVDD.

    可以连接到AVDD。

  • 我将XSMT按照您提的接到AVDD后,使用三线的I2S,SCK接地,主机的I2S信号已经可以测量到,但是Lout和Rout没有波形输出,其他的配置是:FMT,DEMP,FLT均接地,输出的16位,48000Hz的数字音频信号,还有其他地方可以排查吗

  • 我这边试着看了一下您其他的原理图链接,没有看到明显的问题。虽然datasheet建议模拟地和数字地要分开,但我觉得也不会导致一点声音没输出。

    Lout和Rout链接的下级芯片,用的是相同的1.8V电压是吧,如果是,那也没问题。