.请TI工程师确定一下 PCM4204是I2S接口?。如果是I2S,如果与STM32F407连接,是不是PCM的M_CLK对应I2S的MCLK,PCM的LRCK对应I2S的MS,PCM的BCK对应I2S的SCK,PCM的DATA对应I2S的DATA。
如果 PCM4204不是I2S接口,如果与STM32F407连接,该怎么连接。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
芯片数据手册,PCM4204是模拟数字转换芯片,输入音频模拟信号,输出数字音频信号,输出数据格式支持I2S。
PCM4204: High Performance 24-Bit, 216kHz Sampling Four-Chan Audio A/D Converter datasheet (Rev. A) (ti.com) 音频串行口输出包括下面管脚,功能说明在19页“AUDIO SERIAL PORT OPERATION”。
STM32F407非TI产品,请根据下面管脚功能描述连接STM32F407。

请参考数据手册“Table 6”“Table 7”选择I2S模式。
电路设计请参考评估板,原理图在评估板用户手册中。
您好,
如前面回复SDOUT1和SDOUT2是对应不同通道的,选择一个连接,不使用对应通道即可。
如果支持TDM格式,使用SDOUT1(Figure 4)。