This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1808: 模拟输入短接到GND,I2S端底噪数据过大,这怎么解决

Part Number: PCM1808

之前自己做的板子也有底噪问题,后面逛了论坛给出的答案也是说按照DEMO板,后面按照官方给的gerber文件,自行打了DEMO板样板。然后BOM方面也是按照官方的。测试发现当模拟输入的左右声道通过电容短接到地后,I2S端的数据脚脚还是一直有波形,通过逻辑分析仪采集I2S的数据发现,I2S补码值偏高,分析发现模拟通过短接到地数据脚值用到了8位位宽,实际是底噪数据。电源纹波5V是22mv左右 ,3.3V是19mv左右。之现在已经都按照官方的,还是有底噪问题,实在无从下手排查了。

  • 您好,

    底噪每个板子都会有的,但是程度不同,一般都是GND的影响,还有就是EMC的影响,比如,您的I2S输入信号用的线,是否有屏蔽层,看看用带屏蔽层的线是否会好转。

    另外,就是几个板子之间的公地问题,电源,I2S输入信号的基板,这个Demo板,三个需要工地,用的线要短一些,粗一些。

    看看这样是否有一定改善。

    再就是板卡PCB本身的设计,我目测你你照片里的PCB,感觉还是挺好的。

    希望我的回答对您有帮助,谢谢。