This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5707+PCM1808

Other Parts Discussed in Thread: TAS5707A, PCM1808, TAS5707

管理员,您好。最近遇到一个问题,调了两天了,再这请教一下: 我应用MCU去控制PCM1808+TAS5707A实现音频数字功放,我的硬件连接如下: PCM1808的MD1=1,MD0=0,Master mode(384fs) FMT=0,I2S,24-bit LRCK,BCK,DOUT接到TAS5707A的I2S接口 SCK与TAS5707A的MCLK连接在一起,接了一个16.9344M的有源晶振 TAS5707的连接: PDN、FAULT、接MCU的IO口,I2C总线接I2C总线,I2C读写正常 用示波器测试有源晶振16.9344正确, CPM1808 LRCLK-44.1K;BCK-28.8223M;DOUT-324K;SCK-16.9344M TAS5707配置: 上电延时一段,RESET=0;PDN=1;延时300MS;RESET=1; 延时300MS之后向0X1B寄存器写0X00, 延时400MS向0X00寄存器写0X70(MCLK 采样频率 16.9344/384=44.1K分频) 每次上电复位之后,两个喇叭会发出嘟嘟的声音,在这个时候读取错误寄存器0X02 的值是OX32(意思是SCLK/LRCLK时钟错误,过流,超压,低压故障),但这个时候TAS5707A FAULT管脚输出为高,故障应该输出为低。 检查了很久,不知道什么问题,不知知道硬件连接走线有没什么特殊的要求。求教一下。

x 出现错误。请重试或与管理员联系。