This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5711 Slave 模式如何設定2.1聲道程序

請問一下,我目前用了一個DSP+5711的方案,以DSP為Matser,5711為slave模式,看了Design Guide內容的部分,依照參數下去,聲音都沒有輸出,附上我的程式碼檔案,能否告知是哪個環節出了問題,謝謝

  • 你好:

    1.你的原理图连接是否正确?可以对照我们的EVM板检查连接。

    2.没有声音输出的时候,看一下电感前面是不是50%占空比的PWM波形,开关频率是不是384Khz。

    3. 2.1的软件设置主要是0x05寄存器改成0x84或0x8C.

     

     

  • 兄弟 你的问题解决了吗  我用的tas5508 也是没出声 可以讨论下吗Q273203365

  • 我是依照你們EVB板的原理圖去製作的,我現在遇到的問題是2.1模式程式不知道修改什麼地方,我附件中的程序在2.0 BD模式是有聲音輸出的,如你所說,我是只要去修改0x05這邊就好了嗎?還是還有什麼地方也需要修改,煩請告知
  • 我的5508在 2.0也是出声了 现在研究 怎么 分频 让左右声道各输出高低音 初涉音频 感觉好难

  • Hi Flora;

                  現在聲音都出來了,不過我有發現另一個問題,就是我在線路上預留的2.0與2.1的切換,可是目前我的軟件寫的是2.1模式,但是怎麼我的4個輸出接口都會有聲音輸出,另外下列是我的代碼,現在發現2.1模式狀態下,低音的效果都沒出來,是不是我哪邊有沒寫到或是寫錯,麻煩請幫我確認下

    #include "define.h"
    #include "tas57xx.h"
    #include "i2c.h"
    #include "tim4.h"
    #include "vm20xx.h"
    #define I2cmWrite1Byte i2cm_wr
    #define I2cmRead1Byte  i2cm_rd
    #define TAS57XX_GAIN_TBL_NO 31
    
    unsigned char const tas57xx_dgain_tbl[]={
    255,   //0,dgain=-120.0
    106+8, //1+8,dgain=-29.0
    103+8, //2+8,dgain=-27.7
    101+8, //3+8,dgain=-26.3
    98+8,  //4+8,dgain=-25.0
    95+8,  //5+8,dgain=-23.6
    93+8,  //6+8,dgain=-22.3
    90+8,  //7+8,dgain=-20.9
    87+8,  //8+8,dgain=-19.6
    84+8,  //9+8,dgain=-18.2
    82+8,  //10+8,dgain=-16.9
    79+8,  //11+8,dgain=-15.6
    76+8,  //12+8,dgain=-14.2
    74+8,  //13+8,dgain=-12.9
    71+8,  //14+8,dgain=-11.5
    68+8,  //15+8,dgain=-10.2
    66+8,  //16+8,dgain=-8.8
    63+8,  //17+8,dgain=-7.5
    60+8,  //18+8,dgain=-6.1
    58+8,  //19+8,dgain=+8.8
    55+8,  //20+8,dgain=-3.4
    52+8,  //21+8,dgain=-2.1
    50+8,  //22+8,dgain=-0.8
    47+8,  //23+8,dgain=0.6
    44+8,  //24+8,dgain=1.9
    41+8,  //25+8,dgain=3.3
    39+8,  //26+8,dgain=4.6
    36+8,  //27+8,dgain=6.0
    33+8,  //28+8,dgain=7.3
    31+8,  //29+8,dgain=8.7
    28+8,  //30+8,dgain=10.0
    };
    
    unsigned char const sta57xx_BQ1a[]={
    0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00
    };
    unsigned char const sta57xx_BQ1b[]={
    0x00,0x80,0x3E,0x83,0x0F,0x00,0xD8,0x83,0x00,0x7E,0xEB,0xB7,0x00,0xFF,0x27,0x7D,0x0F,0x80,0xD5,0xC5
    };	//Type:eq;fc:60hz   ;Gain4db  ;BW:50hz
    //0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00
    //};	//Type:eq;fc:60hz   ;Gain4db  ;BW:50hz
    unsigned char const sta57xx_BQ1[][20]={
    {0x00,0x7F,0xEF,0x61,0x0F,0x00,0xA2,0x1B,0x00,0x7F,0x6F,0x04,0x00,0xFF,0x5D,0xE5,0x0F,0x80,0xA1,0x9A}, //Type:eq;fc:30hz   ;Gain-2db  ;BW:30hz
    {0x00,0x81,0x3E,0xA0,0x0F,0x00,0xD7,0xC9,0x00,0x7D,0xEB,0x9A,0x00,0xFF,0x28,0x37,0x0F,0x80,0xD5,0xC5}, //Type:eq;fc:60hz  ;Gain12db ;BW:50hz
    {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, //Type:eq;fc:125hz ;Gain:-6db  ;BW:100hz
    {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}, //Type:eq;fc:250hz ;Gain:-4db  ;BW:1500hz
    {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}  //Type:eq;fc:5000hz ;Gain:5db  ;BW:15000hz
    };
    unsigned char const sta57xx_BQ1d[][20]={
    {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00},
    {0x00,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}
    };
    unsigned char const sta57xx_bass[][20]={
    {0x00,0x80,0x00,0x00,0x0F,0x03,0x54,0x5F,0x00,0x7C,0xB1,0x2C,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 0 db  ;BW:200hz
    {0x00,0x80,0x6D,0xA1,0x0F,0x03,0x54,0x5F,0x00,0x7C,0x43,0x8A,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 2 db  ;BW:200hz
    {0x00,0x80,0xF7,0xA6,0x0F,0x03,0x54,0x5F,0x00,0x7B,0xB9,0x85,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 4 db  ;BW:200hz
    {0x00,0x81,0xA5,0x68,0x0F,0x03,0x54,0x5F,0x00,0x7B,0x0B,0xC3,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 6 db  ;BW:200hz
    {0x00,0x82,0x80,0x27,0x0F,0x03,0x54,0x5F,0x00,0x7A,0x31,0x04,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 8 db  ;BW:200hz
    {0x00,0x83,0x93,0x89,0x0F,0x03,0x54,0x5F,0x00,0x79,0x1D,0xA2,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 10 db  ;BW:200hz
    {0x00,0x84,0xEE,0x3A,0x0F,0x03,0x54,0x5F,0x00,0x77,0xC2,0xF2,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 12 db  ;BW:200hz
    {0x00,0x86,0xA2,0xAE,0x0F,0x03,0x54,0x5F,0x00,0x76,0x0E,0x7D,0x00,0xFC,0xAB,0xA1,0x0F,0x83,0x4E,0xD4}, //Type:eq;fc:100hz   ;Gain 14 db  ;BW:200hz
    };
    
    #define DRC  //turn on compressor
    #define EQ_ON //turn on eq
    
    //---------------------------------------------------------------------
    // initialize sta339
    //---------------------------------------------------------------------
    #ifdef PAMP_TAS5711
    void tas57xx_init(void)
    { unsigned long tmp;//becaue STM8 's long is 32bit, int is 16 bits
      unsigned char i;
      //unsigned char *rdats;
      //time delay for BD mode,according to spec
    //---------------------------------------------------------------------
    // 2.0 Both BD Mode
    //---------------------------------------------------------------------
    //  i2cm_wr(TAS57XX_ID,0x1b,0x00); 
    //  i2cm_wr32(TAS57XX_ID,0x20,0x00897772);//both bd mode
    //	i2cm_wr32(TAS57XX_ID,0x25,0x01021345);//both bd mode
    //	i2cm_wr(TAS57XX_ID,0x11,0xb8);
    //  i2cm_wr(TAS57XX_ID,0x12,0x60);
    //  i2cm_wr(TAS57XX_ID,0x13,0xa0);
    //  i2cm_wr(TAS57XX_ID,0x14,0x48);
    //---------------------------------------------------------------------
    // 2.1 BD Mode Output For David Add
    //---------------------------------------------------------------------
    	i2cm_wr(TAS57XX_ID,0x1b,0x00);  // Oscillator Trim
    	i2cm_wr(TAS57XX_ID,0x03,0xa0);  // System Control Register 1
    	i2cm_wr(TAS57XX_ID,0x04,0x05);  // Serial Data Interface Register
    	i2cm_wr(TAS57XX_ID,0x06,0x00);  // Soft Mute Register
    	i2cm_wr(TAS57XX_ID,0x07,0x2a);  // Master Volume Register (0xFF = Mute)
    	i2cm_wr(TAS57XX_ID,0x08,0x30);  // Channel 1 Volume
    	i2cm_wr(TAS57XX_ID,0x09,0x30);  // Channel 2 Volume
    	i2cm_wr(TAS57XX_ID,0x0a,0x30);  // SubChannel Volume
    	i2cm_wr(TAS57XX_ID,0x0e,0x91);  // Micro Register
    	i2cm_wr(TAS57XX_ID,0x10,0x02);  // Modulation Limit
    	i2cm_wr(TAS57XX_ID,0x19,0x30);  // Shutdown Group Resister
    	i2cm_wr(TAS57XX_ID,0x1a,0x95);  // Split Capacitor Charge Period 
    	i2cm_wr(TAS57XX_ID,0x1c,0x02);  // Back-end Error Register
    	i2cm_wr32(TAS57XX_ID,0x20,0x00897772); // 2.1 output mode
    	i2cm_wr32(TAS57XX_ID,0x21,0x00004203);
    	i2cm_wr32(TAS57XX_ID,0x25,0x01013245); //PWM Output MUX Register, OUT_A=PWM1(L+),OUT_B=PWM3(R-),OUT_C=PWM2(SUB+),OUT_D=PWM4(SUB-) 
    	i2cm_wr(TAS57XX_ID,0x11,0xac);  // Inter-Channel Delay Channel 1
    	i2cm_wr(TAS57XX_ID,0x12,0x54);  // Inter-Channel Delay Channel 2
    	i2cm_wr(TAS57XX_ID,0x13,0xac);  // Inter-Channel Delay Channel 3
    	i2cm_wr(TAS57XX_ID,0x14,0x54);  // Inter-Channel Delay Channel 4
    	i2cm_wr(TAS57XX_ID,0x17,0x00);  // Offset Register (Absolute Delay)
    	i2cm_wr(TAS57XX_ID,0x05,0x84);  // System Control Register 2 (active)
     
    //woofer
      //i2cm_wr_eq(TAS57XX_ID,0x29, (unsigned long *)sta57xx_s_lpf1);   #ifdef DRC
       #ifdef DRC
      // //------------------------------------------------------
      // i2cm_wr64(TAS57XX_ID,0x3a,0x000006d3,0x007FF92c);//energe filter=100ms
      // i2cm_wr64(TAS57XX_ID,0x3b,0x00000DA6,0x007FF259);//attack filter=50ms
      // i2cm_wr64(TAS57XX_ID,0x3c,0x0000015D,0x007FFEA2);//decay filter=500ms
      // i2cm_wr32(TAS57XX_ID,0x40,0xFC98537A);//thresh hold=-17db
      // i2cm_wr32(TAS57XX_ID,0x41,0x0FAAAAAB);//ratio=3
      // i2cm_wr32(TAS57XX_ID,0x42,0x00107A1C);//offset(makeup gain)=6
      // i2cm_wr32(TAS57XX_ID,0x46,0x1);//enable drc
       ////------------------------------------------------------
       //i2cm_wr64(TAS57XX_ID,0x3a,0x0000883f,0x007F77c0);//energe filter=5ms
       //i2cm_wr64(TAS57XX_ID,0x3b,0x00004432,0x007Fbbcd);//attack filter=10ms
       //i2cm_wr64(TAS57XX_ID,0x3c,0x000006d3,0x007FF92c);//decay filter=100ms
       //i2cm_wr32(TAS57XX_ID,0x40,0xFC98537A);//thresh hold=-17db
       //i2cm_wr32(TAS57XX_ID,0x41,0x0FAAAAAB);//ratio=3
       //i2cm_wr32(TAS57XX_ID,0x42,0x00107A1C);//offset(makeup gain)=6
       //i2cm_wr32(TAS57XX_ID,0x46,0x1);//enable drc
       //------------------------------------------------------
       //i2cm_wr64(TAS57XX_ID,0x3a,0x00000DA6,0x007FF259);//attack filter=50ms 0707 change
       //i2cm_wr64(TAS57XX_ID,0x3b,0x00004432,0x007Fbbcd);//attack filter=10ms 0707 change
       //i2cm_wr64(TAS57XX_ID,0x3c,0x000006d3,0x007FF92c);//decay filter=100ms 0707 change
       //i2cm_wr32(TAS57XX_ID,0x40,0xFC98537A);//thresh hold=-17db 0707 change
       //i2cm_wr32(TAS57XX_ID,0x41,0x0FAAAAAB);//ratio=3 0707 change
       //i2cm_wr32(TAS57XX_ID,0x42,0x00107A1C);//offset(makeup gain)=6 0707 change
       //i2cm_wr32(TAS57XX_ID,0x46,0x1);//enable drc 0707 change
      // //------------------------------------------------------
       i2cm_wr64(TAS57XX_ID,0x3a,0x0000883f,0x007F77c0); //energe filter=5ms
       i2cm_wr64(TAS57XX_ID,0x3b,0x0002A39A,0x007D5C65); //attack filter=1ms
       i2cm_wr64(TAS57XX_ID,0x3c,0x00004432,0x007FBBCD); //decay filter=10ms
       i2cm_wr32(TAS57XX_ID,0x40,0xFC98537A);            //thresh hold=-17db
       i2cm_wr32(TAS57XX_ID,0x41,0x0FAAAAAB);            //ratio=3
       i2cm_wr32(TAS57XX_ID,0x42,0x00107A1C);            //offset(makeup gain)=6
       i2cm_wr32(TAS57XX_ID,0x46,0x1);                   //enable drc
       //------------------------------------------------------
       //i2cm_wr64(TAS57XX_ID,0x3a,0x0000883f,0x007F77c0);//energe filter=5ms
       //i2cm_wr64(TAS57XX_ID,0x3b,0x0002A39A,0x007D5C65);//attack filter=1ms
       //i2cm_wr64(TAS57XX_ID,0x3c,0x00004432,0x007FBBCD);//decay filter=10ms
       //i2cm_wr32(TAS57XX_ID,0x40,0xFC588B89);//thresh hold=-20db
       //i2cm_wr32(TAS57XX_ID,0x41,0x0FC00000);//ratio=2
       //i2cm_wr32(TAS57XX_ID,0x42,0x000BAA32);//offset(makeup gain)=3
       //i2cm_wr32(TAS57XX_ID,0x46,0x1);//enable drc
       //-----------------------------------------------------
       #endif
       //i2cm_wr32(TAS57XX_ID,0x46,0x1);//enable drc
       
       //filter
       //-----------------------------------L---------------------------------------
       #ifdef EQ_ON
       i2cm_wr32(TAS57XX_ID,0x50,0x10101090);//eq control,all 48K,EQ ON,wr L--> copt to  R,no auto bank switch
    
       i2cm_wrN(TAS57XX_ID,0x29,sta57xx_BQ1a,20);
       i2cm_wrN(TAS57XX_ID,0x2a,sta57xx_BQ1b,20);
       for(i=0;i<5;i++)
         i2cm_wrN(TAS57XX_ID,0x2b+i,sta57xx_BQ1[i],20);//0x2b~2f
       for(i=0;i<2;i++)
         i2cm_wrN(TAS57XX_ID,0x58+i,sta57xx_BQ1d[i],20);
       #endif   
      //-----------------------------------R---------------------------------------
       //i2cm_wrN(TAS57XX_ID,0x30,sta57xx_BQ2a,20);//BQ2a
       //i2cm_wrN(TAS57XX_ID,0x31,sta57xx_BQ2b,20);//BQ2b
       //for(i=0;i<5;i++)
       //  i2cm_wrN(TAS57XX_ID,0x32+i,sta57xx_BQ2[i],20);//BQ2,*GUI adr is wrong. act0x32~0x36.important
       //for(i=0;i<5;i++)
       //  i2cm_wrN(TAS57XX_ID,0x5c+i,sta57xx_BQ2d[i],20);//BQ2d
    	//---------------------------------------------------------------------------
       //enable
       i2cm_wrN(TAS57XX_ID,0x29,sta57xx_bass[2],20);
       i2cm_wr(TAS57XX_ID,0x05,0x00);//sub-ch class-bd
    }
    #endif
    
    void tas57xx_vol(signed char inc) //not complete. gain table for S
    {
      STATE_VOL+=inc;
      if(STATE_VOL>=(TAS57XX_GAIN_TBL_NO-1))
        STATE_VOL=(TAS57XX_GAIN_TBL_NO-1);
      else if(STATE_VOL<=0)
        STATE_VOL=0;
      STATE_TVOL=tas57xx_dgain_tbl[STATE_VOL];//STATE_TVOL is tmp
      i2cm_wr(TAS57XX_ID,0x07,STATE_TVOL);//tas57xx_dgain_tbl[STATE_VOL]);
      //vm20xx_mbass(STATE_TVOL);
    }
    
    void tas57xx_mute(unsigned char tas57xx_mute) //
    { 
      if(tas57xx_mute)
      {
        STATE_TVOL=tas57xx_dgain_tbl[0];   //STATE_TVOL is tmp
        i2cm_wr(TAS57XX_ID,0x07,STATE_TVOL);//tas57xx_dgain_tbl[STATE_VOL]);
      }
      else
      {
        STATE_TVOL=tas57xx_dgain_tbl[STATE_VOL];//STATE_TVOL is tmp
        i2cm_wr(TAS57XX_ID,0x07,STATE_TVOL);//tas57xx_dgain_tbl[STATE_VOL]);
      }
    }
    
    void tas57xx_pwm_off(void) //
    {
      i2cm_wr(TAS57XX_ID,0x05,0x40);//all ch pwdn
      
    }