This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760L: 怎么通过IIC进行音量控制,需要配置哪些寄存器

Part Number: TAS5760L
Other Parts Discussed in Thread: TAS5825M

TAS5760L how do I configure the volume through the IIC, and why does the volume remain unchanged after configuring the 0X03 address?

  • Hi ,How to adjust the volume through the IIC configuration

  • 您好

    /*
    * Driver for the TAS5825M Audio Amplifier
    *
    * Author: Andy Liu <andy-liu@ti.com>
    * Author: Dario Murgia <dario.murgia@alumni.uniroma2.eu>
    *
    * This program is free software; you can redistribute it and/or
    * modify it under the terms of the GNU General Public License
    * version 2 as published by the Free Software Foundation.
    *
    * This program is distributed in the hope that it will be useful, but
    * WITHOUT ANY WARRANTY; without even the implied warranty of
    * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
    * General Public License for more details.
    */

    #include <linux/module.h>
    #include <linux/moduleparam.h>
    #include <linux/slab.h>
    #include <linux/of.h>
    #include <linux/init.h>
    #include <linux/i2c.h>
    #include <linux/regmap.h>

    #include <sound/soc.h>
    #include <sound/pcm.h>
    #include <sound/initval.h>

    #include "tas5825m.h"

    #define TAS5825M_DRV_NAME "tas5825m"

    #define TAS5825M_RATES (SNDRV_PCM_RATE_48000)
    #define TAS5825M_FORMATS (SNDRV_PCM_FMTBIT_S16_LE | SNDRV_PCM_FMTBIT_S20_3LE |\
    SNDRV_PCM_FMTBIT_S24_LE | SNDRV_PCM_FMTBIT_S32_LE)

    #define TAS5825M_REG_00 (0x00)
    #define TAS5825M_REG_03 (0x03)
    #define TAS5825M_REG_0C (0x0c)
    #define TAS5825M_REG_0D (0x0d)
    #define TAS5825M_REG_0E (0x0e)
    #define TAS5825M_REG_0F (0x0f)
    #define TAS5825M_REG_10 (0x10)
    #define TAS5825M_REG_11 (0x11)
    #define TAS5825M_REG_12 (0x12)
    #define TAS5825M_REG_13 (0x13)
    #define TAS5825M_REG_35 (0x35)
    #define TAS5825M_REG_7F (0x7f)

    #define TAS5825M_PAGE_00 (0x00)
    #define TAS5825M_PAGE_0B (0x0b)

    #define TAS5825M_BOOK_00 (0x00)
    #define TAS5825M_BOOK_8C (0x8c)

    #define TAS5825M_VOLUME_MAX (110) //158
    #define TAS5825M_VOLUME_MIN (40) //0

    const uint32_t tas5825m_volume[] = {
    0x0000001B, //0, -110dB
    0x0000001E, //1, -109dB
    0x00000021, //2, -108dB
    0x00000025, //3, -107dB
    0x0000002A, //4, -106dB
    0x0000002F, //5, -105dB
    0x00000035, //6, -104dB
    0x0000003B, //7, -103dB
    0x00000043, //8, -102dB
    0x0000004B, //9, -101dB
    0x00000054, //10, -100dB
    0x0000005E, //11, -99dB
    0x0000006A, //12, -98dB
    0x00000076, //13, -97dB
    0x00000085, //14, -96dB
    0x00000095, //15, -95dB
    0x000000A7, //16, -94dB
    0x000000BC, //17, -93dB
    0x000000D3, //18, -92dB
    0x000000EC, //19, -91dB
    0x00000109, //20, -90dB
    0x0000012A, //21, -89dB
    0x0000014E, //22, -88dB
    0x00000177, //23, -87dB
    0x000001A4, //24, -86dB
    0x000001D8, //25, -85dB
    0x00000211, //26, -84dB
    0x00000252, //27, -83dB
    0x0000029A, //28, -82dB
    0x000002EC, //29, -81dB
    0x00000347, //30, -80dB
    0x000003AD, //31, -79dB
    0x00000420, //32, -78dB
    0x000004A1, //33, -77dB
    0x00000532, //34, -76dB
    0x000005D4, //35, -75dB
    0x0000068A, //36, -74dB
    0x00000756, //37, -73dB
    0x0000083B, //38, -72dB
    0x0000093C, //39, -71dB
    0x00000A5D, //40, -70dB
    0x00000BA0, //41, -69dB
    0x00000D0C, //42, -68dB
    0x00000EA3, //43, -67dB
    0x0000106C, //44, -66dB
    0x0000126D, //45, -65dB
    0x000014AD, //46, -64dB
    0x00001733, //47, -63dB
    0x00001A07, //48, -62dB
    0x00001D34, //49, -61dB
    0x000020C5, //50, -60dB
    0x000024C4, //51, -59dB
    0x00002941, //52, -58dB
    0x00002E49, //53, -57dB
    0x000033EF, //54, -56dB
    0x00003A45, //55, -55dB
    0x00004161, //56, -54dB
    0x0000495C, //57, -53dB
    0x0000524F, //58, -52dB
    0x00005C5A, //59, -51dB
    0x0000679F, //60, -50dB
    0x00007444, //61, -49dB
    0x00008274, //62, -48dB
    0x0000925F, //63, -47dB
    0x0000A43B, //64, -46dB
    0x0000B845, //65, -45dB
    0x0000CEC1, //66, -44dB
    0x0000E7FB, //67, -43dB
    0x00010449, //68, -42dB
    0x0001240C, //69, -41dB
    0x000147AE, //70, -40dB
    0x00016FAA, //71, -39dB
    0x00019C86, //72, -38dB
    0x0001CEDC, //73, -37dB
    0x00020756, //74, -36dB
    0x000246B5, //75, -35dB
    0x00028DCF, //76, -34dB
    0x0002DD96, //77, -33dB
    0x00033718, //78, -32dB
    0x00039B87, //79, -31dB
    0x00040C37, //80, -30dB
    0x00048AA7, //81, -29dB
    0x00051884, //82, -28dB
    0x0005B7B1, //83, -27dB
    0x00066A4A, //84, -26dB
    0x000732AE, //85, -25dB
    0x00081385, //86, -24dB
    0x00090FCC, //87, -23dB
    0x000A2ADB, //88, -22dB
    0x000B6873, //89, -21dB
    0x000CCCCD, //90, -20dB
    0x000E5CA1, //91, -19dB
    0x00101D3F, //92, -18dB
    0x0012149A, //93, -17dB
    0x00144961, //94, -16dB
    0x0016C311, //95, -15dB
    0x00198A13, //96, -14dB
    0x001CA7D7, //97, -13dB
    0x002026F3, //98, -12dB
    0x00241347, //99, -11dB
    0x00287A27, //100, -10dB
    0x002D6A86, //101, -9dB
    0x0032F52D, //102, -8dB
    0x00392CEE, //103, -7dB
    0x004026E7, //104, -6dB
    0x0047FACD, //105, -5dB
    0x0050C336, //106, -4dB
    0x005A9DF8, //107, -3dB
    0x0065AC8C, //108, -2dB
    0x00721483, //109, -1dB
    0x00800000, //110, 0dB
    0x008F9E4D, //111, 1dB
    0x00A12478, //112, 2dB
    0x00B4CE08, //113, 3dB
    0x00CADDC8, //114, 4dB
    0x00E39EA9, //115, 5dB
    0x00FF64C1, //116, 6dB
    0x011E8E6A, //117, 7dB
    0x0141857F, //118, 8dB
    0x0168C0C6, //119, 9dB
    0x0194C584, //120, 10dB
    0x01C62940, //121, 11dB
    0x01FD93C2, //122, 12dB
    0x023BC148, //123, 13dB
    0x02818508, //124, 14dB
    0x02CFCC01, //125, 15dB
    0x0327A01A, //126, 16dB
    0x038A2BAD, //127, 17dB
    0x03F8BD7A, //128, 18dB
    0x0474CD1B, //129, 19dB
    0x05000000, //130, 20dB
    0x059C2F02, //131, 21dB
    0x064B6CAE, //132, 22dB
    0x07100C4D, //133, 23dB
    0x07ECA9CD, //134, 24dB
    0x08E43299, //135, 25dB
    0x09F9EF8E, //136, 26dB
    0x0B319025, //137, 27dB
    0x0C8F36F2, //138, 28dB
    0x0E1787B8, //139, 29dB
    0x0FCFB725, //140, 30dB
    0x11BD9C84, //141, 31dB
    0x13E7C594, //142, 32dB
    0x16558CCB, //143, 33dB
    0x190F3254, //144, 34dB
    0x1C1DF80E, //145, 35dB
    0x1F8C4107, //146, 36dB
    0x2365B4BF, //147, 37dB
    0x27B766C2, //148, 38dB
    0x2C900313, //149, 39dB
    0x32000000, //150, 40dB
    0x3819D612, //151, 41dB
    0x3EF23ECA, //152, 42dB
    0x46A07B07, //153, 43dB
    0x4F3EA203, //154, 44dB
    0x58E9F9F9, //155, 45dB
    0x63C35B8E, //156, 46dB
    0x6FEFA16D, //157, 47dB
    0x7D982575, //158, 48dB
    };

    struct tas5825m_priv {
    struct regmap *regmap;

    struct mutex lock;

    int vol;
    };

    const struct regmap_config tas5825m_regmap = {
    .reg_bits = 8,
    .val_bits = 8,
    .cache_type = REGCACHE_RBTREE,
    };

    static int tas5825m_vol_info(struct snd_kcontrol *kcontrol, struct snd_ctl_elem_info *uinfo)
    {
    uinfo->type = SNDRV_CTL_ELEM_TYPE_INTEGER;
    uinfo->access = (SNDRV_CTL_ELEM_ACCESS_TLV_READ | SNDRV_CTL_ELEM_ACCESS_READWRITE);
    uinfo->count = 1;

    uinfo->value.integer.min = TAS5825M_VOLUME_MIN;
    uinfo->value.integer.max = TAS5825M_VOLUME_MAX;
    uinfo->value.integer.step = 1;

    return 0;
    }

    static int tas5825m_vol_locked_get(struct snd_kcontrol *kcontrol, struct snd_ctl_elem_value *ucontrol)
    {
    struct snd_soc_codec *codec = snd_soc_kcontrol_codec(kcontrol);
    struct tas5825m_priv *tas5825m = snd_soc_codec_get_drvdata(codec);

    mutex_lock(&tas5825m->lock);
    ucontrol->value.integer.value[0] = tas5825m->vol;
    mutex_unlock(&tas5825m->lock);

    return 0;
    }

    static inline int get_volume_index(int vol)
    {
    int index;
    index = vol;

    if (index < TAS5825M_VOLUME_MIN)
    index = TAS5825M_VOLUME_MIN;

    if (index > TAS5825M_VOLUME_MAX)
    index = TAS5825M_VOLUME_MAX;

    return index;
    }

    static void tas5825m_set_volume(struct snd_soc_codec *codec, int vol)
    {
    unsigned int index;
    uint32_t volume_hex;
    uint8_t byte4;
    uint8_t byte3;
    uint8_t byte2;
    uint8_t byte1;

    index = get_volume_index(vol);
    volume_hex = tas5825m_volume[index];

    byte4 = ((volume_hex >> 24) & 0xFF);
    byte3 = ((volume_hex >> 16) & 0xFF);
    byte2 = ((volume_hex >> 8) & 0xFF);
    byte1 = ((volume_hex >> 0) & 0xFF);

    snd_soc_write(codec, TAS5825M_REG_00, TAS5825M_PAGE_00);
    snd_soc_write(codec, TAS5825M_REG_7F, TAS5825M_BOOK_8C);
    snd_soc_write(codec, TAS5825M_REG_00, TAS5825M_PAGE_0B);
    snd_soc_write(codec, TAS5825M_REG_0C, byte4);
    snd_soc_write(codec, TAS5825M_REG_0D, byte3);
    snd_soc_write(codec, TAS5825M_REG_0E, byte2);
    snd_soc_write(codec, TAS5825M_REG_0F, byte1);
    snd_soc_write(codec, TAS5825M_REG_10, byte4);
    snd_soc_write(codec, TAS5825M_REG_11, byte3);
    snd_soc_write(codec, TAS5825M_REG_12, byte2);
    snd_soc_write(codec, TAS5825M_REG_13, byte1);
    }

    static int tas5825m_vol_locked_put(struct snd_kcontrol *kcontrol, struct snd_ctl_elem_value *ucontrol)
    {
    struct snd_soc_codec *codec = snd_soc_kcontrol_codec(kcontrol);
    struct tas5825m_priv *tas5825m = snd_soc_codec_get_drvdata(codec);

    mutex_lock(&tas5825m->lock);

    tas5825m->vol = ucontrol->value.integer.value[0];
    tas5825m_set_volume(codec, tas5825m->vol);

    mutex_unlock(&tas5825m->lock);

    return 0;
    }

    static const struct snd_kcontrol_new tas5825m_vol_control =
    {
    .iface = SNDRV_CTL_ELEM_IFACE_MIXER,
    .name = "Master Playback Volume",
    .info = tas5825m_vol_info,
    .get = tas5825m_vol_locked_get,
    .put = tas5825m_vol_locked_put,
    };

    static int tas5825m_snd_probe(struct snd_soc_codec *codec)
    {
    int ret;

    ret = snd_soc_add_codec_controls(codec, &tas5825m_vol_control, 1);

    return ret;
    }

    static struct snd_soc_codec_driver soc_codec_tas5825m = {
    .probe = tas5825m_snd_probe,
    };

    static int tas5825m_mute(struct snd_soc_dai *dai, int mute)
    {
    u8 reg03_value = 0;
    u8 reg35_value = 0;
    struct snd_soc_codec *codec = dai->codec;

    if (mute)
    {
    reg03_value = 0x0b;
    reg35_value = 0x00;
    }
    else
    {
    reg03_value = 0x03;
    reg35_value = 0x11;
    }

    snd_soc_write(codec, TAS5825M_REG_00, TAS5825M_PAGE_00);
    snd_soc_write(codec, TAS5825M_REG_7F, TAS5825M_BOOK_00);
    snd_soc_write(codec, TAS5825M_REG_00, TAS5825M_PAGE_00);
    snd_soc_write(codec, TAS5825M_REG_03, reg03_value);
    snd_soc_write(codec, TAS5825M_REG_35, reg35_value);

    return 0;
    }

    static const struct snd_soc_dai_ops tas5825m_dai_ops = {
    .digital_mute = tas5825m_mute,
    };

    static struct snd_soc_dai_driver tas5825m_dai = {
    .name = "tas5825m-amp",
    .playback = {
    .stream_name = "Playback",
    .channels_min = 2,
    .channels_max = 2,
    .rates = TAS5825M_RATES,
    .formats = TAS5825M_FORMATS,
    },
    .ops = &tas5825m_dai_ops,
    };

    static int tas5825m_probe(struct device *dev, struct regmap *regmap)
    {
    struct tas5825m_priv *tas5825m;
    int ret;

    tas5825m = devm_kzalloc(dev, sizeof(struct tas5825m_priv), GFP_KERNEL);
    if (!tas5825m)
    return -ENOMEM;

    dev_set_drvdata(dev, tas5825m);
    tas5825m->regmap = regmap;
    tas5825m->vol = 85; // -25dB

    mutex_init(&tas5825m->lock);

    ret = regmap_register_patch(regmap, tas5825m_init_sequence, ARRAY_SIZE(tas5825m_init_sequence));
    if (ret != 0)
    {
    dev_err(dev, "Failed to initialize TAS5825M: %d\n",ret);
    goto err;

    }

    msleep(5);
    ret = regmap_register_patch(regmap, tas5825m_init1_sequence, ARRAY_SIZE(tas5825m_init1_sequence));
    if (ret != 0)
    {
    dev_err(dev, "Failed to initialize TAS5825M: %d\n",ret);
    goto err;

    }


    ret = snd_soc_register_codec(dev,
    &soc_codec_tas5825m,
    &tas5825m_dai,
    1);
    if (ret != 0)
    {
    dev_err(dev, "Failed to register CODEC: %d\n", ret);
    goto err;
    }

    return 0;

    err:
    return ret;

    }

    static int tas5825m_i2c_probe(struct i2c_client *i2c, const struct i2c_device_id *id)
    {
    struct regmap *regmap;
    struct regmap_config config = tas5825m_regmap;

    regmap = devm_regmap_init_i2c(i2c, &config);
    if (IS_ERR(regmap))
    return PTR_ERR(regmap);

    return tas5825m_probe(&i2c->dev, regmap);
    }

    static int tas5825m_remove(struct device *dev)
    {
    snd_soc_unregister_codec(dev);

    return 0;
    }

    static int tas5825m_i2c_remove(struct i2c_client *i2c)
    {
    tas5825m_remove(&i2c->dev);

    return 0;
    }

    static const struct i2c_device_id tas5825m_i2c_id[] = {
    { "tas5825m", },
    { }
    };
    MODULE_DEVICE_TABLE(i2c, tas5825m_i2c_id);

    #ifdef CONFIG_OF
    static const struct of_device_id tas5825m_of_match[] = {
    { .compatible = "ti,tas5825m", },
    { }
    };
    MODULE_DEVICE_TABLE(of, tas5825m_of_match);
    #endif

    static struct i2c_driver tas5825m_i2c_driver = {
    .probe = tas5825m_i2c_probe,
    .remove = tas5825m_i2c_remove,
    .id_table = tas5825m_i2c_id,
    .driver = {
    .name = TAS5825M_DRV_NAME,
    .of_match_table = tas5825m_of_match,
    },
    };

    module_i2c_driver(tas5825m_i2c_driver);

    MODULE_AUTHOR("Andy Liu <andy-liu@ti.com>");
    MODULE_AUTHOR("Dario Murgia <dario.murgia@alumni.uniroma2.eu>");
    MODULE_DESCRIPTION("TAS5825M Audio Amplifier Driver");
    MODULE_LICENSE("GPL v2");

    这是给您分享的帖子中的相关代码,有关于音量配置的代码,请您参考一下。

x 出现错误。请重试或与管理员联系。