This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV632: DRV632 uvp Pin 设计指南确认

Part Number: DRV632


关于DRV632的UVP外围电阻设计有如下疑问

1.UVP的关断电压是1.25V,在外部检测电阻设计中有两个设计公式中提出有一个6uA和一个5uA,这两个电流值分别是哪里流到哪里的电流?是分别流向R2和R3吗?那样的话,流过R1的电流不就是11uA?

2.如果是根据问题1的电流大小,那在For example中,当R1=3K,R2=1K时,Vuvp=3.8V时,电阻的电流是远大于11mA的

3.如果我系统电压是24V或者是3.3V,R1,R2,R3应该设计多少?能否指教设计过程,谢谢!