This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5715两个DRC的运用问题

TI技术员您好:

   对于TAS5715两个DRC的运用有一个问题,DRC1的入口寄存器0X40确定后,无论怎么调DRC2的入口寄存器,压限值都是和DRC1是一样的,0X50的D4位也设置为0,0X59,0X5D为高通或低通buttonworth2  3000HZ,

  我现在要用一个TAS5715做一个高音和一个低音,希望高音输出电压在8V,频率在3000HZ以上,低音输出在10V,频率在3000HZ