This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3131无输出



输入信号3.3V  ~400K,mute、SD有FPGA管脚控制。

GVDD只有0.64V,而不是手册的7V,所以plim、GAIN/FLvt得到的分压为0,我猜想是这里的问题导致的!

但是GVDD应该是内部LDO产生的,AVDD/PVCC均供的7.5V,为什么GVDD还是没有输出呢?

是芯片问题还是其他有什么要配置产生吗?

谢谢