This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254的MIC相关

大家好:

现在调试通过3200控制3254
 问题是MIC端的振动很小。

现在测得mic串联电容相关参数
AUDBOOST:电容与MIC连接端电压为800mV左右,有语音振动幅度为±200mV左右
                   电容与芯片连接端电压为900mV左右有语音振动幅度为±100mV左右
产品电路板中:电容与MIC连接端电压为600mV左右,有语音振动幅度非常小
                   电容与芯片连接端电压为900mV左右有语音振动幅度几乎看不到

电容增大或者舍去测试过,效果类似,振动幅度很小。AUDBOOST中的MIC也被换成我们自己的MIC。

2.2k电阻测得相关参数
AUDBOOST:电阻与MIC连接端电压为0.783V左右 
                   电阻与芯片连接端电压为1.242V左右
产品电路板中:电阻与MIC连接端电压为0.609V左右
                   电阻与芯片连接端电压为1.239V左右

这个电压值是否也有影响。
这个是电路图