This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6422E-Q1: TAS6422E-Q1 output inductor L limited value when PWM=384/480k

Part Number: TAS6422E-Q1


In the datasheet of TAS6424, we can see

“The selection of a 2.11 MHz switch frequency enables the use of a small output inductor value of 3.3 μH

which leads to a very small solution size.”

So, if it means we can not use the one of minimum value 3.3uH when pwm frequency is selected 384KHz?

What inductor value limited can be used with PWM 384KHz with 2ohm load if F response(20~20kHz) results can be permitted within a large range?