Part Number: TAS6424E-Q1
Hello, I have a few questions about this chip that I would like to ask.
When the TAS6424E is configured for line-output mode, whether operations such as volume control are the same as in normal mode or not, the difference is only that the two modes have different initial configurations for the 0X00 register.
2. When the chip is configured for line output mode, can it be understood that the chip is used as an audio DAC? If it is used as a DAC, does the internal decoding result in an audio output filter that is the same as the one specified in the chip datasheet? Is an additional low-pass filter (LPF) circuit needed, and if so, can you recommend a circuit?
3) Could you recommend some DAC chips with similar TAS6424 chip decoding capabilities but without the power amplifier section, capable of decoding 32-bit audio data?
Above, please find my questions. Thank you for your response.