This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC6140EVM-PDK: adc6140evm-pdk

Part Number: ADC6140EVM-PDK
Other Parts Discussed in Thread: TLV320ADC6140

adc6140evm-pdk 系列开发板能否用于接收放大640hz-200khz的频率信号,放大信号接USB输出信号是什么格式,需要用上位机程序解码吗

  • 您好,

         tlv320adc6140芯片输入信号频率最高80 kHz(数据手册  8.3.6 Signal-Chain Processing,

         但adc6140evm-pdk由于48KHZ采样率的原因,可以支持到20KHZ.(评估板用户手册 2.1.1.2 Optical or Auxilary Analog Audio Input)

         USB音频格式可以是TDM或I2S格式.