Other Parts Discussed in Thread: TAS5825P
Total output power: 500W = Woofer 150W*2 + Tweeter 50W*4
Can we choose 2*TAS3251+4*TAS5825P ?
I'm not sure if it makes sense to use 6 devices.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This is a possible option if digital input is needed, but a few changes can be made.
First, the TAS3251 can output 175W into 3 Ohms in BTL mode so no need for two devices in PBTL. Just make sure they do decent thermal designing.
Second, if a pad down device is necessary, then the TAS5827 could be used which can do 55W output into two 4 ohm speakers (10%THD), but thermals will be trickier to manage due to pad down nature. Because the customer is already using a heatsink for the TAS3251, I would recommend the TAS5828M which can do the 2x50W no problem since it uses a heat sink.
Regards,