This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116D2: 功放这边100~200MHZ辐射偏高

功放在100~200mhz的情况下,辐射偏高,看有没有办法解决?

  • 您好

    #数据手册图34是辐射发射测试结果,因为铁氧体磁珠的阻抗主要在10-100MHz有效,但是传导发射频带为150kHz~30MHz,所以如果您需要同时实现“通过传导发射”和“使用铁氧体珠滤波器(低成本)”,那将是一个很大的挑战。

    #TPA311X使用电感器作为滤波器,可以顺利通过传导发射和辐射发射。
    #使用铁氧体磁珠作为滤波器,截止频率为几MHz,PWM能量将通过扬声器线。但客户可以选择铁氧体磁珠(阻抗较大)来降低PWM边缘速率,另一种降低边缘速率的方法是增加电容器(例如,将1000pF改为2200pF)。

    可以基于这款芯片的评估板的原理图和layout进行调整。

    https://www.ti.com/tool/TPA3116D2EVM