This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
TPA3251在BTL模式下需要差分输入,不能像TPA3128一样将单端输入转为差分信号。
在BTL(Bridge-Tied Load)模式下,TPA3251的两个输入信号是差分输入。这意味着,与某些其他芯片(如TPA3128可能具有的功能)不同,TPA3251在BTL配置下不支持将单端输入信号直接转换为差分信号。因此,如果需要使用TPA3251在BTL模式下工作,必须提供差分输入信号。
TPA3251是一款高性能音频放大器,支持多种输出配置,包括双声道Stereo BTL输出配置。该芯片具有差分模拟输入等特性,并且具有高速栅极驱动器错误校正功能,能够提供高质量的音频放大效果。
如果尝试在BTL模式下使用单端输入信号,可能会导致芯片无法正常工作或性能下降。因此,为了确保TPA3251在BTL模式下的最佳性能,建议遵循数据手册中的说明,使用差分输入信号。
这是官方详细显示请您参考。