This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5711 Mixer如何设定

Other Parts Discussed in Thread: TAS5711

用TAS5711做2.1声道,按照默认的设置得到的结果总是感觉声音都偏左边了,调整EQ没有什么改善,是否Mixer需要修改?如何修改?另外这些Mixer该如何理解呢?请TI的工程师大大帮忙解答一下,现在的设置如下:

0x05 84
0x20 00-01-77-72
0x21 00-00-42-03
0x25 01-01-32-45
0x53 00-80-00-00-00-00-00-00-00-00-00-00-00-80-00-00
0x54 00-80-00-00-00-00-00-00-00-00-00-00-00-80-00-00
0x51 00-80-00-00-00-00-00-00-00-00-00-00
0x52 00-80-00-00-00-00-00-00-00-00-00-00
0x60 00-40-00-00-00-80-00-00

  • 结果总是感觉声音都偏左边了,感觉往往不是真得. 也许扬声器也有问题

    你可以用仪器测量一下

  • 不是喇叭或者硬件的问题,已经测量过,2.1的低音单元在中间,Lowpass设定在300以下,当Mixer60两个通道的值设定为1:1的比例,右声道混入低音单元的量明显多于左声道,所以会有这个听感,不知道该怎么正确的设置这些Mixer,这些Mixer对所有channel的影响分别是怎样的?,我找不到比较详细的一些说明资料,希望能有人帮忙解答