你好,针对于自己设计的PCB,我有两个疑问
1:不使用PPCMB,如何能把我的板子连上purepath.
2:我手动写的程序,为啥在page0和page1都是能正常读写的, 但是换到别的page,比如说page44,就不能直接写入的,我是想尝试把贵司提供的linux代码写进去,但是发现很多页没有写成功,读出来全是0
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,针对于自己设计的PCB,我有两个疑问
1:不使用PPCMB,如何能把我的板子连上purepath.
2:我手动写的程序,为啥在page0和page1都是能正常读写的, 但是换到别的page,比如说page44,就不能直接写入的,我是想尝试把贵司提供的linux代码写进去,但是发现很多页没有写成功,读出来全是0
谢谢
没有PPCMB或EVM,就无法与自定义板通信。您至少需要PPCMB才能获取I2C信号发送给您的rend系统。至于页面,可能是您正在访问的页面不存在,或者所讨论的注册表是只读的。
你好,
1,我的理解是就需要一个USB转IIC的就能连接上我的板子,那么符合USB转IIC的转换板,是不是也行。
2,同时我看你们的PPCMB原理图上USB那儿就只有一个TAS1020B,然后贵司官网好像也有TAS1020B的固件用于IIC,是不是我做个这样的接口板也可以。
3,我希望的就是一根线,或者一个很小的接口板就能连上我的设计,而不是用PPCMB这么大的板子,麻烦看看是否行得通, tks
可以用其他的。
TAS1020B已经停产,所以你需要一个不同的解决方案来进行这样的转换。