This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA1637的模拟输入具有以下共模电压要求。由于Vcc=5Vdc和Vee=-10Vdc,因此总Vs=15Vdc。
负电源轨必须加1V,正电压轨必须减去1V-->这使得输入Vcm的范围为-9V和4Vdc。Δ电压为-13Vdc,中点为-6.5Vdc。因此,-9Vdc-(-6.5Vdc)=-2.5Vdc(从负轨的角度来看)。4V-6.5V=-2.5Vdc(从正极轨道的角度来看)。
无论如何,如果Vcc=5Vdc和Vee=-10Vdc,-2.5V将是输入共模电压的中点。中点是输入信号的幅度可以从Vocm等量摆动。
对于Vocm控制,建议从任一电源轨获得+/-2V。
为了使输入电压摆动最大化,最佳Vocm参考电压为(-8V-3V)/2=-5.5Vdc。
从正电压轨的角度来看,3Vdc-5.5Vdc=-2.5Vdc
从负电压轨的角度来看,-8Vdc-(-5.5Vdc)=-2.5Vdc
中点或最佳Vocm应为-2.5Vdc,但-3.5Vdc也适用于电源轨。
TPA3151中还有另一个要求,其最大输入电压摆动为7V-->因此这也可能是一个考虑因素。顺便说一句,我不熟悉TPA3151部分,所以我的猜测是Vocm应该在电源轨和输入共模电压的中点进行优化。