Part Number: TAS5825M
Hello TI team,
when I ultilized the TAS5825M as the woofer(PBTL mode, Mono Output), I noticed that the output volumes for left channel input and right channel input are not equal.
Specifically, when I play with an audio file with only left channel, the output volume was quite higher than that when I played with right channel file.
I tried to adjust the input mixer register but nothing changed.
The following details outline my initialization settings for the woofer.
0x00 0x00
0x7f 0x00
0x03 0x02
0x01 0x11
0x00 0x00
0x00 0x7f
0x7f 0x00
0x7d 0x11
0x7d 0xff
0x00 0x01
0x51 0x05
0x00 0x02
0x19 0xa0
0x1d 0x01
0x00 0x00
0x7f 0x00
0x46 0x01
0x00 0x00
0x02 0x44 // PBTL MODE
0x53 0x60
0x00 0x00
0x7f 0x00
0x03 0x02
DELAY 6 ms
0x00 0x00
0x7f 0x00
0x03 0x03
I don't know why there is an issue of imbalance between the left and right channels. The volume generated by the right channel is much lower than that of the left channel.
Many thanks in advance.