Part Number: TLV320AIC3104
现在我们3104做一块核心板,线性差分输入到差分输出,如图是原理图和PCB:



用AP做音频测试,测试出来只有72dB的信噪比,采样率是22050,麻烦帮忙看一下如何做才能提高信噪比到92dB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320AIC3104
现在我们3104做一块核心板,线性差分输入到差分输出,如图是原理图和PCB:



用AP做音频测试,测试出来只有72dB的信噪比,采样率是22050,麻烦帮忙看一下如何做才能提高信噪比到92dB
您好,
感谢您的报告。 我理解问题,也有几个问题。
92dB号仅特定于ADC。 通过运行差分输入到差分输出的测试,您将增加来自DAC的额外噪音。
还有一个问题,即100mV是任意的,与我们测量数据表SNR的方式不匹配。
要重新创建SNR测试,请将两个模拟输入短接至GND,并在PGA增益为0dB时测量ADC输出(I2S输出)的dBFS值。 该值为SNR,应接近92dB。
在DAC端可以执行相同的测试。 在DAC通电的情况下,移除输入信号(I2S)并测量有效值输出。 此值应作为设备满刻度输出的dB测量值。 SNR = 20log(x/1.414),其中x是测得的rms输出。