Other Parts Discussed in Thread: PCM2912A
现做一款USB声卡,求音频控制芯片
Rev.2.0 high-speed/full-speed模式兼容
bit depth / sampling rate :24Bit/192KHz以上。
求各大神帮找找。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCM2912A
现做一款USB声卡,求音频控制芯片
Rev.2.0 high-speed/full-speed模式兼容
bit depth / sampling rate :24Bit/192KHz以上。
求各大神帮找找。
USB2.0 没问题,24bit也没问题,但是好像没有192KHz以上的,USB codec好像最大为48KHz,像PCM2912A.
这说这种我有查找看到,
所以我在找 USB控制主芯片。
Savitech的SA9226能满足24Bit/32Bit/192k,DSD要求
谢谢推荐。这款我了解了一下,功耗比较大,3.3V工作电流达到了80MA呢,要是再加上codec的话超过IPhone(输出100MA)就带不动了也许。
下面你还推荐了一款NUC42的查了一下,特性:
[• ADC
- 12位ADC(最多16通道)
- 最快速度1 MSPS】
它的ADC部分是不是达不到24Bit。
还有推荐的吗?
你是做DAC还是ADC呀,功能连PC还是手机,ios or android,USB口还是Lightning口呢?
DAC/ADC都要有,功能是连接PC,IOS or android 。是支持USB2.0的但对于IOS和Android来说使用OTG连接即可。
谢谢,这个推荐是不错的。不过SA9227还不知道他的功耗,不知道手机能带的动不。
看音频输出的功率,30+30mW以内问题不大,应在100mA以内,SA9227有两路I2S,可以取消AK4556.
具体视你做什么用途。