新增加的R228和R229这两个电阻可以把偏置电压上拉到-0.2V,不知道会不会有什么影响?
TRANSLATE with x
English
TRANSLATE with
Enable collaborative features and customize widget: Bing Webmaster Portal
Back
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

新增加的R228和R229这两个电阻可以把偏置电压上拉到-0.2V,不知道会不会有什么影响?
新增加的R228和R229这两个电阻可以把偏置电压上拉到-0.2V,不知道会不会有什么影响?
这是 PGA2405EVM 参考设计。 差分输入信号是在 CC1和 CC2节点已经进行平衡之前的信号、请参阅随附的图像和链路。 使用 C162和 C163以及 R228和 R229存储区居中显示差分信号可能无法解决

https://www.ti.com/lit/ug/sbou078/sbou078.pdf?ts=1743065177092
如果-0.2V 偏置电压是由 R228和 R229产生的、则意味着 R225和 R229不匹配良好。 它是-0.2V 稳定的直流偏置电压吗? 从技术上讲、如果是共模电压、差动运算放大器的 CMRR 应将其大部分移除。 C162和 C163之间的电容可能会存在更多变化或不匹配、从而导致输入不平衡。 如果您有其他问题、敬请告知。
它是-0.2V 稳定的直流偏置电压吗?
是的,这-0.2V是稳定的直流偏置电压。增加的这两个电阻( R225和 R229),强行把-0.65V的直流偏置(输入引脚偏置到大约(VcoMIN-0.65V))拉到-0.2V。
从技术上讲、如果是共模电压
是的,这只是有-0.65V的电压被上拉到-0.2V的共模电压
C162和 C163之间的电容可能会存在更多变化或不匹配、从而导致输入不平衡。
说明书的第9页右下角的倒数第二段有提到:It is recommended that a small capacitor be connected from each analog input pin to analog ground. Values of at least 50pF are recommended.See Figure 10 for larger capacitors used for EM filtering, which satisfies this requirement.
可以在输入引脚增加50pF的小电容到GND,目的为了增加EMI滤波,那现在增加的C162和C163会影响到输入信号吗?会导致输入不平衡吗?但,目前我有测了输入信号的波形,没影响的。
它是-0.2V 稳定的直流偏置电压吗?是的,这-0.2V是稳定的直流偏置电压。增加的这两个电阻( R225和 R229),强行把-0.65V的直流偏置(输入引脚偏置到大约(VcoMIN-0.65V))拉到-0.2V。从技术上讲、如果是共模电压、差动运算放大器的 CMRR 应将其大部分移除。是的,这只是有-0.65V的电压被上拉到-0.2V的共模电压,会影响到CMRR吗?
C162和 C163之间的电容可能会存在更多变化或不匹配、从而导致输入不平衡。说明书的第9页右下角的倒数第二段有提到:It is recommended that a small capacitor be connected from each analog input pin to analog ground. Values of at least 50pF are recommended.See Figure 10 for larger capacitors used for EM filtering, which satisfies this requirement.
可以在输入引脚增加50pF的小电容到GND,目的为了增加EMI滤波,那现在增加的C162和C163会影响到输入信号吗?会导致输入不平衡吗?但,目前我有测了输入信号的波形,没影响的。
如果这是直流、则 PGA2505中的 CMRR 对于音频应用应至少为80dB (可能为100dB 或更高)。 假设它为80dB、则运算放大器将抑制约-0.2/80dB =-0.2/10000的噪声、这约为-20uV。 如果 CMRR = 100dB、则将仅为-2uV。 我不相信人类能听到不同的声音。 您可以使用音频分析仪进行检查和验证。
这似乎是可以接受的。 10Ω 和200pF 是共模滤波器、截止频率用于滤除潜在的 EMI 噪声。 差分滤波器为20Ω 和50pF、它们尝试滤除 EMI 中的剩余差分噪声。 两个滤波器与音频输入信号没有直接关系、音频输入阻抗应在高达20kHz 的频率下保持平衡。