Pin10,Pin11,Pin12不一致,都是在一份规格书中,分别是5页与78页,请问是什么问题,我如果采用硬件模式,该怎么用?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
没看出有什么问题, P78是把hardware mode 和software mode的引脚集合在一起。
datasheet的P2和P5是分开标注的引脚。

我查询了一下,以前有客户问过类似的问题。
是有些差异,我在去问下这个芯片的设计工程师,看看是不是P5的引脚定义有误。
下面是工程师的回复。
Actually, the three pins are GPIO, and the function could be defined by register 0x61(GPIO1/ pin11 ), 0x62(GPIO2/ pin12 ), 0x63(GPIO0/ pin10 ).

and of course, you can also use PPC3 to config it like below which is the default setting of 48k stereo mode: